STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 with a 50.0MHz Oscillator

Posted on March 20, 2018 at 19:00I am running an STM32F407 with an ECS-2033-500BN Oscillator (50.0MHz) to accommodate the MCU and the ETH off the same oscillator. The circuit uses a fanout buffer to distribute the clock. Nowhere can I find informati...

ST7735 display driver usage

Posted on March 07, 2018 at 08:10Hi .I have a LCD display with st7735 and wanted to use library included within STM32Cube_FW_F3_V1.8.0 package.Unfortunately the lib seems to be written only for specific boards and while compiling the code I get erro...

Rad Rad by Associate II
  • 3567 Views
  • 2 replies
  • 0 kudos

UART stm32f4 discovery board

Posted on March 20, 2018 at 16:20hi, i need to recive variable amoun of data from the UART, but the problem is that the pointer of the Rx buffer is incremented any time and i cant decrease it, sorry for my english, i working whit stm32f4 discovery b...

Flash PGSERR PGPERR continious raised

Posted on March 21, 2018 at 12:24Hi,try to erase and write to Flash on STM32F407. Get after a hardware reset always raised PGSERR PGPERR Error Flags.After resetting the values, the mentioned Error Flags will be raised after passing the next code lin...

Nucleo-L496ZG in 1.8V

Posted on March 21, 2018 at 10:52Hello,I have a nucleo-L496zg board (stm32L496ZgT6 144 pins) and I'd like to use it in 1.8V.From the document UM2179, section 6.5.4 I see that it's possible depending of the connection on SB121, SB122and SB127, which ...

Setting up sim800 with stm32f103c8

Posted on March 20, 2018 at 12:43hi i'm trying to set up a gsm sim800 module with stm32f103c8 .i want to switch a led on and off with sms . i used stm32cubemx for usart settings and i generated a code for that.. now i want to recieve sms with at com...

salar s by Associate
  • 5557 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.