STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer Interrupt not working on STM32F103C8

Posted on April 04, 2018 at 14:51I am using CubeMX and SW4STM32 to generate timer update interrupt on STM32F103C8. The core is running at 64 MHz, and I have verified that other functions like GPIO, PWM, ADC work perfect.The target is to generate an ...

STM32L452 SystemClock_Config with STM32CubeMX

Posted on April 03, 2018 at 12:27Hi,I have Nuckeo-L452RE with STM32L452RE uC on board.This uC max speed is 80MHz.But after enabling MCO on pin PA8 in STM32CubeMX and generating the code to Atollic, I could see wrong SYSCLK frequencies.The reason of ...

Where are _IRQHandler functions defined?

Posted on March 04, 2017 at 16:13Ok so I am talking about the IRQ handlers for ADC, SPI, I2C USART etc.. I am expecting to see weak definitions of ADC_IRQHandler() function for example somewhere...but my startup_stm32.s file in startup directory doe...

NUCLEO-F767ZI Demo Software

Posted on April 04, 2018 at 16:58Where can I find the source of the demo software which is already loaded on a 'fresh from the box' NUCLEO-F767ZI please. I searched the forum and looked on the ST nucleo web pages already.Thanks - John F.

John F. by Senior
  • 2155 Views
  • 3 replies
  • 0 kudos

Resolved! USART3 voltage level

Posted on April 04, 2018 at 22:31I'm using STM32F207ZG ,What is maximum Voltage level at Tx and Rx pin in USART3? Can I use 5V CP2102  USB to TTL converter with STM32F207ZG?

STM32 PMSM foc sdk 5.0 serial communication

Posted on April 05, 2018 at 04:11I am working with stm32 PMSM foc sdk 5.0. I want to drive the system by the application board and it can send a command to the motor drive board and get a feedback.The application board and motor drive board communic...

HAL_FLASH_OB_Launch(), holding..

Posted on April 05, 2018 at 03:50Hi.I am going to set the RDP-Level 1 programmatically.Here is the test code:Here it stops at the HAL_FLASH_OB_Launch () function.The Reset button does not work in this state.The USB connection will work only if you r...

Jin ho An by Associate II
  • 1060 Views
  • 0 replies
  • 0 kudos

STM32F303VCT6 ADC input imedance

Posted on April 05, 2018 at 02:00What is the ADc input impedance on the  STM32F303VCT6? How to decide of ADC input sampling time? My signal is very low frequency (10 kHz).Please let me know.Channamallesh

''USB On-The-Go Host'' or ''USB Host''?

Posted on April 02, 2018 at 23:30Hi everyone,I'm working on a board based on STM32F4XX. We plan to support USB Host on it for communication(CDC). I found there are 'USB On-The-Go Host' and 'USB Host' libraries. I'm not sure which one to use.First, I...

Pilot B by Associate II
  • 2167 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.