STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F777VI USB enumeration fails with DMA enabled

Posted on April 04, 2018 at 18:29We have the STM32F777VI in HS USB mode using external ULPI. We are using the CDC virtual com port (VCP) example with V1.2.5 HAL Driver and V2.4.2 USB Device Library. Without DMA everything works fine. But as soon as ...

0690X0000060APyQAM.png
jr by Associate II
  • 1726 Views
  • 2 replies
  • 0 kudos

Resolved! GPIO_D pin 9 remains ''high''

Posted on April 05, 2018 at 03:06 Hey everyone, I'm using a nucleo f722ze which has an onboard stm32f722ze. The problem: GPIO_D pin 9 remains above 1.5 V even when it's set as off(''reset state''). Every other pin I've used and tested doesn't...

0690X00000604YVQAY.jpg
con3 by Senior
  • 2085 Views
  • 4 replies
  • 0 kudos

how to extract data from ethernet at the reception

Posted on March 28, 2018 at 09:51Hello im using stm32f429ZI NUCLEO (with server application netconn) , protocol tcp for sending and receiving data using ethernet ,, i can send no prblm , i receive also but i need to save like a serie , i use this se...

First project in Nucleo-f429zi using TrueStudio

Posted on March 12, 2018 at 14:31Hello, I am new on Nucleo-F429zi and truestudio. After I installed truestudio and download stm32cube_fw_f4_v1.19.0. I found pretty examples in folder projects, so I try GPIO, but after  I open this project in truestu...

yang hong by Associate III
  • 761 Views
  • 1 replies
  • 0 kudos

Increase the intensity of white led

Posted on April 04, 2018 at 17:29Hi , I want to drive White Led 7 Segment Display. MCUs power supply is 3.3V (STM32F030C6T6), and white led voltage about 2.8V when the current is 20mA. So, light intensity is too low. Is there any way to increase int...

Resolved! CubeMX : Adding Additional expansions

Posted on April 04, 2018 at 18:17How can I add STs expansion packs. http://www.st.com/en/embedded-software/stm32cube-expansion-packages.html?querycriteria=productId=LN1920 But how can I add them, a timer tool could be useful.There was a thread about...

LMI2 by Lead
  • 1010 Views
  • 1 replies
  • 0 kudos

FMC-SDRAM

Posted on April 03, 2018 at 07:49Hello, I will use FMC for SDRAM. I looked examples and tried. But this examples used Bank2, I want to use Bank1. How can I do ?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.