STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 External power supply issue

Posted on July 04, 2016 at 16:43Hi all,I'm working with an STM32F429 disco board and I can't seem to get it to work with an external power supply (USB cable not plugged in). When connected via USB, everything is functioning as required. I have one o...

max239955 by Associate II
  • 3168 Views
  • 8 replies
  • 0 kudos

Modify of HAL library?

Posted on April 09, 2018 at 08:33HI,I use SPI of HAL Library in STM32F0.However, due to unaligned memory access, HardFault occurs in the HAL_SPI_TransmitReceive () function.So I modified the HAL library as follows.uint8_t data_lo, data_hi;uint16_t d...

UART baudrate problem

Posted on April 08, 2018 at 20:15Hello,I try to send data via UART with a baudrate 8Mb/s using Nucleo-L476RG and UM232H,the programs I use are STM32CubeMx and Putty (for RX)As shown on the picture below we can send data via USART1 with a baudrate be...

0690X0000060ATcQAM.png 0690X0000060ATgQAM.png 0690X0000060AUFQA2.png

STM32H7 Triple ADC Conversion Not Supported

Posted on March 16, 2018 at 02:22Hi All,Contrary to what the http://www.st.com/resource/en/application_note/dm00337702.pdf document says about the H7 chip, it does not support Triple ADC Conversion mode. It only supports double conversion mode betwe...

JacobV by Associate II
  • 1294 Views
  • 1 replies
  • 0 kudos

Clk Configuration problem

Posted on April 10, 2018 at 12:43Hi, the problem is not solved, below is the clock configuration, Based on the figure above, I tried to use the different divisions /1, /8.. and the different clk (PPLCK, SYCLK, HSE...)  to obtain the correct frequenc...

0690X0000060AVrQAM.png 0690X0000060AVmQAM.png 0690X0000060AKuQAM.png 0690X0000060AVwQAM.png

[STM32L073RZT6] Read USB pins from GPRS modem

Posted on April 03, 2018 at 13:33Hello everybody,I would like to read the USB_DM and USB_DP pins from a GPRS module (it only works in Device mode) with the STM32L073RZT6 microcontroller which has also USB pins available. However, I realized that it ...

STM32F429 Cortex M4 MPU Crash Freertos

Posted on April 10, 2018 at 10:27Hi,We have been trying to use ARM_CM4F_MPU port in one of our application. Freertos version is 10.0.0.An unprivileged task always Mem Faults when trying to use a kernel API though mpu_wrappers is elevating the privil...

Mit N by Associate
  • 760 Views
  • 0 replies
  • 0 kudos

Fatfs f_close causes idle hook

Posted on April 09, 2018 at 08:38Hello everyone I use stm32f746 discovery board. I implemented emwin,Free rtos and Fatfs for the SDcard(using SDIO interface). In my application after pressing a button, a value(as a string) is saved in the SDcard....

Resolved! Debug stuck in LL_RCC_PLL_IsReady

Posted on April 09, 2018 at 16:58 Hello, I have a Nucleo-L476RG and I am trying to debug using openocd. I am able to reach main() function, but when it calls SystemClock_Config() get stuck in:while(LL_RCC_PLL_IsReady() != 1) The firmware...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.