STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f070xB, TIM16_CH1 input capture

Posted on April 23, 2018 at 12:59I am using STM32f070xB controller. I want to use @TIM16_CH1 for input capture.GPIO_PIN: ♯PB8Timer clock freq: 3MHzTIMER is getting interrupted continuously but after 120Hz, flow is not going into Capture compare call...

STM32 SMBus Read Byte Error

Posted on April 23, 2018 at 08:54I used ST supply STM32_AN4502_FW_V2.0.2 for SMBus.When  test Read Byte command?0x19 can work?but 0x00 can not ACK right,TIMEOUT happen,Why?#smbus

What is the best way to use the serial device in this case?

Posted on April 23, 2018 at 18:08I am currently using a driver that uses latch and clock signals to send special commands before sending data. For the sending of the data the driver works as for an SPI but with the signal of clock. Here is the diagr...

0690X00000604alQAA.jpg
Jems On by Associate III
  • 3305 Views
  • 7 replies
  • 0 kudos

Is internal RC clock stable enough?

Posted on April 24, 2018 at 10:53Hi,I am planning to use STM32F301K8 with UFQFPN32 package (the PCB space is critical).I am going to use:1 or 2 UARTs in Asynchronouse mode driven by DMA. 8N1 . Boud Rate 115200 .1 or 2 SPIs driven by DMA. Csn by not ...

ADC values via UART on STM32L011

Posted on April 24, 2018 at 11:40Hello Friends!I am very new to STM coding and starting with the basics. I am using a STM32L011 uC and IAR compiler.I am trying to measure voltage from a sensor that is dumping analog data at about 5Khz. The ADC value...

0690X0000060AkcQAE.png 0690X0000060AkhQAE.png
Sid by Associate II
  • 6735 Views
  • 8 replies
  • 0 kudos

CRC-32 on F4/F7

Posted on June 27, 2016 at 16:07Just thought I'd save people some time if they are trying to get the CRC engine on the F4/F7 to produce the same results as most online calculators. If you are using CubeMX to configure your CRC, you need to specify t...

kevin2399 by Associate III
  • 3750 Views
  • 5 replies
  • 2 kudos

HAL_FLASH_Program behavior

Posted on April 24, 2018 at 17:35I came across a rare issue where a previously failed flash operation would cause a subsequent operation to fail as well.  I tracked it down to stm32f4xx_hal_flash.c::HAL_Flash_Program()When the function calls FLASH_W...

Setting UART baud rate to 600

Posted on April 24, 2018 at 10:13Hi,I'm trying to set the UART baud rate to 600 on a Nucleo F070RB board to communicate with the CS5490 chip. (https://www.cirrus.com/products/cs5490/)I've only managed to go down to 732 baud rate. Anything below, it ...

CAN on STM32F429-DISCO board

Posted on March 25, 2018 at 16:45Hello, I have question about CAN on STM32F429-DISCO board.I found that CAN1 is shared with display control and CAN2 with on-chip debugger. In comments for this video (/external-link.jspa?url=https%3A%2F%2Fwww.youtube...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.