STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Uploading code / PWR Jumper - What am I doing wrong?

Posted on May 03, 2018 at 10:39I am quite new to STM32 and never worked with a Nucleo before.  I am trying to control two motors (from a hoverboard) with a Nucleo F446RE. I found a perfect example with libraries and example code on GitHub, but someh...

Interfacing Max232 with stm32

Posted on May 03, 2018 at 14:00I'm working with stm32vldiscovery and I'm going to use max232 for USART. I'm using usart1 (pA9 and pA10 as TX and RX).The question is witch is the best way to make it wortk correctly and safetly specially with the RX p...

Problem with STM32F427 and spurious EXTI interrupts

Posted on April 11, 2017 at 22:31I use the following code to initialize the GPIO for EXTI interrupt handling.I want GPIO F14 to trigger on the falling edge and most of the time it works properly.However, every 1000 or so interrupts, the EXTI Interru...

Can both microphones and Line In audio input channels on STM32F769I DISCO board be used simultaneously for 2 different audio sources?

Posted on April 30, 2018 at 06:27STM32F769I DISCO board has 2 input options (mics and line in) and 2 output options (headphones and speaker). According to the examples in the CUBE package, we have the option to use both outputs simultaneously. Is it...

flashing stm32F303 based custom board

Posted on May 03, 2018 at 23:36Hello,I am making a custom board based on STM32F3 discovery board. My custom board is an exact copy of the discovery board with additional sensor components. I can easily program STM32F3 board as st-link is already bui...

STM32L4 register setting

Posted on May 03, 2018 at 19:43I'm trying to program STM32L4-discovery board using the registers of ST32L4 only. I wanted to modify flash latency and see if the register value really changes by using gdb. However, it turned out that the following si...

M. Jeong by Associate II
  • 824 Views
  • 2 replies
  • 0 kudos

Cubemx 4.25 STM32F767 EXTI problem

Posted on April 03, 2018 at 20:44I've configured a number of pins on the 767 as EXTI but there is no option in NVIC to enable the interrupts and no code generated. The pins are correctly identified in  the GPIO configuration tab.Moreover, the exampl...

Using ll_sdmmc.c with eMMC

Posted on April 25, 2018 at 16:40Hi,I�m working on a project with the STM32L4 on a custom board. We want to access a eMMC to store acquired data. First, we used the HAL_sd.c library, but since it�s not compatible with eMMC, we now want to use the lo...

Maxim H by Associate
  • 1141 Views
  • 1 replies
  • 0 kudos

How to get SiLabs CP2102N working as a USB device?

Posted on May 03, 2018 at 18:03Hello,I'm working on a board based on STM32F427 MCU. The board is implemented as a USB Host.I'm trying to get SiLabs' CP2102N working as a USB device. I understand I'll need to change the driver to make it work. Have a...

Pilot B by Associate II
  • 695 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.