STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX linker RAM section wrong size?

Posted on May 10, 2018 at 10:37 Hi folks, I just looked at the linker script generated by CubeMX for a STM32F205RB. The bits I'm concerned about; /* Highest address of the user mode stack */ _estack = 0x20010000; /* end of RAM */ /* Gener...

Is the STM32H7 intended to replace F7 family?

Posted on January 31, 2018 at 16:50Is the STM32H7 intended to replace F7 family? I want to start a design and considered the F7 family but will it disappear when the H7 is in full production?#stm32h7 #stm32f7

John F. by Senior
  • 9167 Views
  • 11 replies
  • 0 kudos

SPI - DMA - NUCLEOH743ZI

Posted on May 16, 2018 at 20:06In NUCLEO-H743ZI  environment using the STM32CubeMX the:HAL_SPI_Receive_DMA(&hspi1, (uint8_t*)u8SpiRxBuffer, SIZE) function in Master Mode.It generates the clocks on the output pin correctly up to 16 byte of data.If th...

Need help with CRC unit

Posted on May 10, 2018 at 09:28STM32L452CMy code:__HAL_RCC_CRC_CLK_ENABLE(); CRC->POL = (uint32_t) 0x1021;//CRC-16-CCITT CRC->INIT = (uint32_t) 0xFFFF; CRC->CR = (uint32_t) 0x09;//REV_OUT = 0, REV_IN = 00, POLYSIZE = 01, RESET = 1 CRC->DR = '1'; CRC...

SVD files - SPI4 on STM32F303ZE, STM32F302XE

Posted on May 15, 2018 at 19:44The .SVD files (https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fresource%2Fen%2Fsvd%2Fstm32f3_svd.zip) for the STM32F303ZE and STM32F302XE seem to be incorrect with respect to the SPI4 IRQn, R...

STM32CubeMX + STM32F746G-DISCO

Posted on March 30, 2018 at 20:42I'm trying to get working code from STM32CubeMX on STM32F746G-DISCO board. I'm using LwIP TCP/IP stack (which works fine - obtains IP address over DHCP) and STemWIN GUI library and there is the problem. LTDC has been...

zenobik by Associate II
  • 2416 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F412G-DISCO arduino pin assignment error

Posted on May 09, 2018 at 15:46When I create a project in CubeMX 4.25.0 with the STM32F412G-DISCO board, the arduino pin assignments are all wrong.I have attached a partial screenshot of the CubeMX project showing the incorrect assignment and a scre...

0690X0000060B5pQAE.png 0690X0000060B6jQAE.png

Power On reset behavior of STM32L071KZU3

Posted on May 16, 2018 at 16:29             We are using STM32L071KZU3 MCU in our design and providing 1.8V to VDD,VDDIO2 and VDDA domains of MCU.         The on-board source voltage to MCU is exactly 1.78V(instead of 1.8V). During power-up, we coul...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.