STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

uint32_t Buttons_GetState (void) explanation?

Posted on May 16, 2018 at 22:42Hi All,Just saw the BSP for buttons on Keil, came across this, can anyone explain how this actually works when one presses the button.Apparently if one was supposed to press button say at pin 13 in this case, GPIOC->ID...

stemwmin and IAR8.20

Posted on May 04, 2018 at 02:51I use in my application the stemwin (STemWin540_CM4_OS_IAR.a) with IAR compiler. Up to version 7.8 of the IAR compiler I never had any warning or error during the build of the project. Upgrading the IAR IDE to version...

STM32f105 UVC host

Posted on May 17, 2018 at 09:07Hi guys, I have used stm32f105RC as host to connect to the UVC camera, now I have got some USB data on the PC, then I want to add this sequence to stm32f105RC project. But now, I can not GET_CUR and SET_CUR.And the cod...

0690X0000060KoSQAU.png 0690X0000060KoNQAU.png 0690X0000060KohQAE.png 0690X0000060KocQAE.png
cable gu by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos

TFT on STM32, use STM32CubeF4 or STemWin or what's current?

Posted on May 09, 2018 at 20:20Hi, I am starting on a new project using a 3.5' 320 x 240 TFT that has an SSD1963 controller. I need to select a processor for this and it seemed like a good chance to use an ARM, but so many choices!  It looks like th...

Grant Bt by Senior II
  • 2142 Views
  • 4 replies
  • 1 kudos

Resolved! HSE ON cleared after HSE RDY set to HIGH?

Posted on May 01, 2018 at 19:05in RCC_CR register does the HSE ON bit gets cleared or not after HSE RDY bit is set to high by MCU? For ex.Set by user:-  17th Bit             16th Bit  HSE RDY [ 0 ],  HSE ON [ 1 ]         //set by userHSE RDY [ 1 ], ...

Resolved! SD_Read bug?

Posted on November 29, 2017 at 14:53 Good day everyone, I'm not sure if this is a bug or I'm looking at this incorrectly, but It seems to be a bug. While calling the f_mount function there is a point where SD_read is called. DRESULT SD_read(B...

0690X00000604DJQAY.jpg
con3 by Senior
  • 7089 Views
  • 14 replies
  • 0 kudos

STM32H7 and heap location

Posted on February 26, 2018 at 19:38I am porting our application from a STM32F779 to a STM32H753 device. Our application looks to run fin if we have the heap located on the DTCM_RAM  (the whole 128k is reserved for heap allocation).If the heap is mo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.