STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem LibJPEG jcdctmgr.c

Posted on June 01, 2018 at 03:31Hello,several days ago I'm trying to encode a BMP image to jpeg, when I do debbug I see that in the jcdctmgr.c file, in the GLOBAL (void) function jinit_forward_dct (j_compress_ptr cinfo)  function, an error occurs at...

STM32H743 FLASH reprogramming

Posted on June 01, 2018 at 12:10Hi,I am porting some firmware from STM32F2 to STM32H743 which is known working good on STM32F205.I am trying to reprogram internal FLASH on BANK1 while executing code from internal RAM. All routines needed in flash.c ...

Get Standby Mode wake up source?

Posted on June 01, 2018 at 12:16I'm putting my STM32L0 in Standby Mode and it can be woken up either by an RTC timer event or by WKUP Pin. Is there a way to check what the source was of the wakeup event? (So check if wakeup was because of WAKEUP pin...

STM32H7 I/O port characteristics

Posted on May 23, 2018 at 11:32Hello, I�m struggling understanding the I/O static characteristics for the STM32H7 devices.I think that below 0.3xVdd a normal input is low and above 0.7xVdd it is high. But what is the meaning of the red marked lines?...

0690X00000604h9QAA.jpg

P-L496G-CELL01 - price & availability?

Posted on February 14, 2018 at 20:15Hi,Does anybody know when this module will be available and how will be priced?http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-eval-tools/stm32-mcu-eval-tools/stm32-mcu-d...

Resolved! STM32L4R5ZI reset issue.

Posted on May 31, 2018 at 15:48Archive addition leading to Reset.Now its failing in SystemClock_Config.And entering to WWDG_IRQHandler() at startup_stm32l4r5xx.s:132 0x8009dc0Failing at RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_OscInitTypeDef ...

CubeMX F4 LL GPDSC code generation issues

Posted on December 14, 2017 at 09:26Hi,I've run into some problems when generating and then importing a GPDSC project when using LL drivers only.Environment: Visual Studio 2017 + VisualGDB (includes STM32CubeMX GPDSC importer)STM32CubeMX V4.23STM32C...

parsec by Associate III
  • 1298 Views
  • 1 replies
  • 0 kudos

X-CUBE-MEMSMIC with 4 channel microphone problem

Posted on October 26, 2017 at 16:51hi, I have  a stm32l476 necleo-64 board and CCA02M1 extension board. I want to modify the the Microphones_Streaming example. and I want to use it to record 4 channel microphone and with 48000Hz sample rate. and I j...

0690X00000608f2QAA.png 0690X00000608lOQAQ.png 0690X00000608jJQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.