STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLinkv2.1 comm error for SWD on STM32469I-Eval

Posted on June 07, 2018 at 07:49Hi,I have STM32469I-Eval board.I used STM32SW4 (AC6) toolchain and built a LED toggle project and debugged it using OpenOCD.Everything was working good.Then i did HW modifications on it by removing CN2, CN4, R216, R21...

STM32429 CAN bus Transmitt Mailbox not trasnmitting?

Posted on June 07, 2018 at 00:42I'm trying to implement the sample code \stm32cube_fw_f4_v1210\STM32Cube_FW_F4_V1.21.0\Projects\STM324x9I_EVAL\Examples\CAN\CAN_Networking\Src on a STM32F429 Nucleo board. Using CubeMx. Single board for now. No transc...

kaveh k by Associate II
  • 4027 Views
  • 5 replies
  • 0 kudos

STM32F7 QSPI Erase and Write (with DMA) Too Slow

Posted on June 07, 2018 at 04:00Hi, all,I have already implemented the configuration of QSPI working in QUAD mode, and DMA2. I want to ready and write about 15M Byte data with QSPI flash. The time cost for reading data is about 2s. However, the time...

nucleo-144stm32f429 usb otg fs

Posted on June 06, 2018 at 21:58Hello, I check stm32cube-fw-f4-v1.21 library for nucleo-144stm32f429zi, I can't find a sample for usb-otg-fs, does anybody be able to provide a sample?also when I try to configure nucleo-144stm32f429zi in stm32cube, I...

yang hong by Associate III
  • 648 Views
  • 1 replies
  • 0 kudos

uart/usart communication

Posted on June 06, 2018 at 22:01I am using nucleo-144stm32f429zi uart and usart. I want to create a rs485 serial communication. Can I connect FTDI USB-RS485-WE-1800-BT directly to nucleo-144 uart/usart port? FTDI CABLE IS 5VDC? nucleo-144stm32f429zi...

yang hong by Associate III
  • 550 Views
  • 1 replies
  • 0 kudos

Ethernet Layer 2 Broadcast

Posted on June 04, 2018 at 20:29Hello Everyone,I need help to send data packets on Ethernet but i want to broadcast it to all the other device on network. For now i want to send hardcoded data which later could be changed. In STMcubeMx i've checked ...

Resolved! STM32L4x6 GPIO PA3 Reset Value

Posted on June 01, 2018 at 15:36 Hi guys, I'm having some troubles understanding the behavior of the ST GPIO on start-up, specifically PA3 on STM32L496VE micro. Background: I'm trying to program/flash a SiLabs BT121 (Bluetooth module) chip an...

0690X0000060KwwQAE.png 0690X0000060L4VQAU.png 0690X0000060L4MQAU.png 0690X0000060KskQAE.png

How to manage SPI transmission using RTX

Posted on June 06, 2018 at 16:30Hello  stI try to use stm32f746 nucleo  as slave controller with raspberry pi3  I use spi as communication method for metal bare code there is no any problem but when I put code in a thread for communication then I fa...

egywell by Associate II
  • 642 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.