2018-06-06 10:49 PM
Hi,
I have STM32469I-Eval board.
I used STM32SW4 (AC6) toolchain and built a LED toggle project and debugged it using OpenOCD.
Everything was working good.
Then i did HW modifications on it by removing CN2, CN4, R216, R217, R227, R228, R6, R15,
R80, R87, R93, R103, R107, R113, R203, R290. On JP14 used PSU, as I am using external power adaptor 5V/2A, came with the kit.
Now I am not able to connect/program the EVal board using ST-Link
utility 4.2.0.0 (with FW version: V2J30M19) and getting this error in trace log:
ST-Link/V2 device detected
Target voltage detected: 3.216787
Error getting target IDCODE: if SWD, check SWD connection
Error (4) while initializing ST-Link in SWD mode
ST-Link/V2 device detected
Target voltage detected: 3.216787
Error getting target IDCODE: if SWD, check SWD connection
Error (4) while initializing ST-Link in SWD mode
ST-Link/V2 device detected
Target voltage detected: 3.216787
Error getting target IDCODE: if SWD, check SWD connection
Error (4) while initializing ST-Link in SWD mode
ST-Link/V2 device detected
Target voltage detected: 3.216787
Error getting target IDCODE: if SWD, check SWD connection
Error (4) while initializing ST-Link in SWD mode
USB communication error (65567) after target cmd F2 45 00 00 FC 00 00 00 00 00
USB communication error (65567) after target cmd F1 80 00 00 00 00 00 00 00 00
ST-Link get version failure
What would be the reason for this failure?
Regards,
Prashant
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.