STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USART Additional features?

Posted on June 26, 2018 at 08:17Using STM32F0xx USART to communicate simplex in standard asynchronous mode (8 bits + parity) with many STM32F0xx slaves. Want to use additional USART features. Did understand and can use Idle and Break detection.What ...

JuM by Senior
  • 582 Views
  • 0 replies
  • 0 kudos

stm32f1 UART and CDC works same for receiving string inside mcu single char receive store in buffer and so on til end char

Posted on June 26, 2018 at 04:07in programming stm32f103cbt6 how can i receive complete string in mcu  send by pc using VCP driver?uart recive char store in buffer so on till end char same process for cdc receive string data?or any other solution fo...

Problem with STEVAL- IHP007V1

Posted on June 26, 2018 at 04:05I have two problem with  STEVAL- IHP007V11. I can't  find pin of connector in schematic of this evaluation board here https://www.st.com/resource/en/schematic_pack/steval-ihp007v1_schematic.pdf 2. User manual of STEVA...

0690X0000060LTaQAM.png
Hung Le by Associate
  • 743 Views
  • 0 replies
  • 0 kudos

Writing multiple blocks to SD card fails

Posted on August 02, 2017 at 14:19Hello. I am developing application that involves writing multiple blocks (of 512 bytes) to SD card. It is a part of USB MSC application, multiblock operations are required for correct and fast functioning. A BSP_SD_...

Ivan Ivan by Associate II
  • 1979 Views
  • 3 replies
  • 0 kudos

stm32 I2C3 master: wont transfer data

Posted on June 26, 2018 at 00:02I am having difficulty transmitting on my stm32l071k8. I am using a STM32l073RZ nucleo board for benchtop development.my lab setup is just a nucleo board connected to an oscilloscope for SCL and SDA. Currently my devi...

Resolved! USB Host on USB-IF Compliance Program

Posted on June 22, 2018 at 01:44Hello,We implemented USB Host on a product based on STM32F427 MCU. Now we try to test it on USB-IF compliance program. But it fails to satisfy the USB-IF requirements.Questions we have:1. Does USB Host support USB Hub...

Pilot B by Associate II
  • 2004 Views
  • 2 replies
  • 0 kudos

Did I break my 407 with +5V?

Posted on June 26, 2018 at 01:12I accidentally used a 5V regulator instead of 3.3V. After fixing that the SWD dongle/ST link says no connection to target. This happens to be my only prototype now. Building a new or swapping the 100pin STM32F407 isn'...

LMI2 by Lead
  • 1054 Views
  • 1 replies
  • 0 kudos

I2C issue with STM32H7 MCU

Posted on June 11, 2018 at 19:14Hello.,., I am using STM32H7 newly released MCU in our project,  In this 3 slave devices are connected thorough I2C interface (Audio codec,EEPROM,RTC devices), All slave devices are accessible and working fine with ro...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.