2018-06-25 4:12 PM
I accidentally used a 5V regulator instead of 3.3V. After fixing that the SWD dongle/ST link says no connection to target. This happens to be my only prototype now. Building a new or swapping the 100pin STM32F407 isn't fun. Has anyone experience of this kind of situation. The absolute maximum VDD is 4.0V.
I have checked SWD connections and Boot0 is pulled low.
2018-06-25 4:48 PM
sorry to say, but Yes I think you are correct.
put 3v on it, does it get hot ? definately faulty.
To remove the chip
you have to get the underside on the board hot
my rework station has the bottom heater and what looks like a paint stripper on top.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.