2018-06-11 10:14 AM
Hello.,.,
I am using STM32H7 newly released MCU in our project, In this 3 slave devices are connected thorough I2C interface (Audio codec,EEPROM,RTC devices), All slave devices are accessible and working fine with room temperature , But when we tested the same unit with 70 Celcius temperature The I2C link become unreliable . Can anyone suggest what could be done to resolve this issue I tried by changing I2C clock in both higher and lower values (Currently I2C clock @ 100KHZ) but end up with same status.
Also during analysis I observed a bug with the Micro controller(STM32H765BIT), A default 200KHZ is generated from contoller (Through PIN 101, same pin i am using as I2C clock pin ), even I erased the complete the flash still by default clock is coming out (I cross checked by removing VCC from MCU , that time clock is not coming ) , I suspecting This could be the one reason that makes I2C unreliable.
Can some STM people spare some time to resolve this issue , We stuck on this issue for long time, Any small help would be appreciated lot.
Thank you.,
#stm32 #i2c-isues2018-06-25 9:40 AM
Hi
karthikshivanna.94
,To more understand your issue, could you please add more details:
1- could you please precise the device you are using? In
family, only lines H743 and H753 are available.2- How exactly is I2C link unreliable at 70°C?
3- Are you using your own hardware or an ST board?
4- What other peripherals than I2C are being used?
5- When seeing a 200KHz on pin 101: is this behaviour observed only at 70°C? are you sure that the flash is really erased? check again using STLink Utility.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-06-25 12:56 PM
Hello.,
I am really sorry , I was totally confused , the default click is coming from some external pheriperal at higher temperature not from MCU , .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.