2018-07-26 8:02 PM
Hi.
Have you ever compile code with error: More than one section matches selector - cannot all be FIRST/LAST.
I searching on google I see that the error because when appear two file same startup_stm32f746xx.s in Startup file and Divice File. I'm delete one file in Start up file and compile again but it's doesn't work.
Please help me with this problem.
Thank you so much.
2018-07-26 8:17 PM
This is going to be hard to diagnose without looking at the project, the files inside, and the scatter file
2018-07-28 12:37 AM
Thank you for your support. I complete to solve this problem.
2018-07-28 7:40 AM
"I complete to solve this problem."
nice. that's going to be very helpful to the next person running into this problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.