STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with using LCD with FMC in SRAM mode. STM32H743.

Hello, Everyone!I found issue with using my LCD (via i8080 mode) with FMC. My display requires HOLD after DATA set from 15 ns time. But in all FMC modes HOLD fixed and it 1 FMC CLK. For my STM32H743 at 400 MHz - I set FMC clock 200 MHz. It is HOLD = ...

STM32F103 I2C Busy flag

Posted on May 22, 2018 at 18:44Hi to all.I'm trying to use I2C peripheral of STM32F103C8T6. I'm using a BluePill board. First of all, I know that this problem was published in other forums and so, but after trying other solutions, I didn't find the ...

SDMMC Data Timeout Error

Posted on April 30, 2018 at 18:19HiI'm trying to write some test data to SD card by DMA with Nucleo-F767Zi.Every 100ms I write 20 blocks to SD card by calling the HAL_SD_WriteBlocks_DMA() method.I have a counter to record how many times the HAL_SD_W...

New forum lacking return links

When I make a post, I have to click at least three links to get back here. Hitting the back button only brings me to some sort of "ping timeout" page. Please either increase the timeout, or provide links back to the top. Links back to anywhere fro...

STM32L4A6VGT power consumption?

Hi,I am measuring a STM32L4A6VGT board power consumption. From the datasheet, in standby mode should be 120nA while I got the value @ 19 mA (last Friday). The FW does nothing, in main after MX_XXX init, call HAL_PWR_EnterSTANDBYMode(). Now I am gett...

STM32 FatFS SDIO DMA bug

Posted on June 14, 2018 at 23:28How to reproduce:1) Use STM32Cube FW_F4 V1.21.0 (not tested on other versions)2) Set up SDIO 1-bit mode with default parameters.3)4) Set up FatFS with SDIO driver with default parameters.5) Set 'Use dma template'=enab...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.