2018-04-30 9:19 AM
Hi
I'm trying to write some test data to SD card by DMA with Nucleo-F767Zi.Every 100ms I write 20 blocks to SD card by calling the HAL_SD_WriteBlocks_DMA() method.I have a counter to record how many times the HAL_SD_WriteBlocks_DMA() have been called since the power up.The HAL_SD_ERROR_DATA_TIMEOUT error interrupt rise up after hundreds calls , sometime several calls.
I read the reference manual.
It says 'When transmitting data, the timeout occurs if the DPSM stays in the Busy state for longer than the programmed timeout period'.I wonder what should I do to prevent the HAL_SD_ERROR_DATA_TIMEOUT error?
------------------------------------------------------------
The clock of SDMMC is 24Mhz. The SD card is Sony 16GB class 4.SDMMC configuration is:
SDHandle_SDMMC.Instance = SDMMC2;SDHandle_SDMMC.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;SDHandle_SDMMC.Init.ClockBypass = SDMMC_CLOCK_BYPASS_DISABLE;SDHandle_SDMMC.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;SDHandle_SDMMC.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_ENABLE;SDHandle_SDMMC.Init.ClockDiv = 0;The related interrupt code in HAL_SD_IRQHandler is:
……else if(__HAL_SD_GET_FLAG(hsd, SDMMC_IT_DCRCFAIL | SDMMC_IT_DTIMEOUT | SDMMC_IT_RXOVERR | SDMMC_IT_TXUNDERR) != RESET){ /* Set Error code */ if(__HAL_SD_GET_FLAG(hsd, SDMMC_IT_DCRCFAIL) != RESET) { hsd->ErrorCode |= HAL_SD_ERROR_DATA_CRC_FAIL; } if(__HAL_SD_GET_FLAG(hsd, SDMMC_IT_DTIMEOUT) != RESET) { hsd->ErrorCode |= HAL_SD_ERROR_DATA_TIMEOUT; } if(__HAL_SD_GET_FLAG(hsd, SDMMC_IT_RXOVERR) != RESET) { hsd->ErrorCode |= HAL_SD_ERROR_RX_OVERRUN; } if(__HAL_SD_GET_FLAG(hsd, SDMMC_IT_TXUNDERR) != RESET) { hsd->ErrorCode |= HAL_SD_ERROR_TX_UNDERRUN; }……2018-08-08 2:08 PM
Can't help you, bumping you off my feed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.