STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Difficulties running sample project - STSW-STM32152

I am trying to get the example 'STSW-STM32152' working for my 32L0538DISCOVERY kit and am having difficulties with the provided projects in the source (v1.0.0) -- TrueSTUDIO (v9.0.1) - No Compile   project linking appears corrupted (see 'TrueSTUDIO C...

Justin1 by Senior
  • 1715 Views
  • 8 replies
  • 0 kudos

Touch panel design with STM32

Hello,I am beginner of stm32, help me with selection of touch MCU & Free IDE from STM32.How to design hardware touch panel with STM32 ?Thank you

TouchMe by Associate
  • 2038 Views
  • 3 replies
  • 0 kudos

stm3240g eval board

Hiis there anyone who has an example where you use the display screen on borad stm3240g-eval and it should be suitable for eclipse

Resolved! STM32F070CBT6 SysTick_Handler never called

Hi all,I have a custom board I have designed with an STM32F070CBT6 on it. Currently it is only populated with the power regulator, one led hooked up to pin PA1 and the debug header.I've used STM32CubeMX to generate a simple test project that initiali...

JFitz.241 by Associate II
  • 1775 Views
  • 2 replies
  • 0 kudos

Nucleo-H743ZI: Strange behavior of CANFD-Controller!

Hi together,I have two Nucleo-Boards with same sw and same external HW. On one HW I get RX acknoledge errors, on the other one everything is fine.Nucleo-H7 with STM32H743ZIOn-Chip CANFD-Controller, CANFD1 (PA11, PA12) and CANFD2 (PB13, PB12)Own exter...

RMehl by Associate
  • 1158 Views
  • 1 replies
  • 0 kudos

Why are all MAC callback functions in I-CUBE-LRWAN moved to lora.c ("inside the stack") and statically defined? (in Stackforce this is not the case)

While working on a standard OTAA Rejoin procedure for our application I've noticed the LoRaMAC callback primitives are all fixed in the LORA_Init() function. When I want to catch the event the MAC layer signals the reception (or not) of a server ACK ...

ingpjb by Associate
  • 800 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.