2018-09-03 10:58 AM
Hi
is there anyone who has an example where you use the display screen on borad stm3240g-eval and it should be suitable for eclipse
2018-09-03 11:43 AM
Some of the Applications, and the Demonstraion in [STM32Cube_FW_F4_V1.15.0]\Projects\STM324xG_EVAL\ ?
> should be suitable for eclipse
How is suitability for eclipse be defined? Both SW4STM32 and TrueStudio are based on Eclipse.
JW
2018-09-04 6:15 AM
just so it works with eclipse
and yeah som of them, where do i find them ?
thanks
2018-09-04 6:30 AM
The examples can be found by unpacking the CubeF4 archive
https://www.st.com/en/embedded-software/stm32cubef4.html
These will be unpacked under the CubeMX repository, if you are using that.
You'll be responsible for importing the projects into the IDE of your choice. As Jan notes SW4STM32 is Eclipse based. Not super popular amongst the commercial programmers here.
STM32Cube_FW_F4_V1.21.0\Projects\STM324xG_EVAL\Applications\Display\LCD_Paint\readme.txt
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.