STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32 - using sd card with SDIO or SPI

Posted on April 26, 2018 at 14:52Hi guys, Im new to stm32 and i have a trouble using sd card with https://www.waveshare.com/wiki/Micro_SD_Storage_Board. I use CubeMX to generate code, and Workbench to edit it. I tried to use my sd card with SPI or S...

How to reduce Data loss on Ping test on STM32F407?

We are facing data loss issue while ping test was conducted on the STM32F407 with lwip stack 1.4.1 The stack was downloaded for  STM32F407 Evaluation Board Code from www.st.com site after changing pin configuration [used tftpserver standalone code] f...

NChen by Associate II
  • 1491 Views
  • 4 replies
  • 0 kudos

No PWM output using TIM1_CH3 on STM32F769 with Keil5.25

Hi i want to enable pwm output on PA10, as in below code, will do necessary init by MX_TIM1_Init, and then call HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3); to start.but PA10 is kept low measured by Osi.could you help review and any suggestion ? thanks...

qzha by Associate II
  • 1830 Views
  • 6 replies
  • 0 kudos

Hello Generating a Pulse Train of 0-200kHz on STM32L476 Nucleo. I Used the Timer to Generate The PWM of a specific Frequency.. That was successful

int main(void) { /* USER CODE BEGIN 1 */ uint16_t Prescaler=1; /* USER CODE END 1 */   /* MCU Configuration----------------------------------------------------------*/   /* Reset of all peripherals, Initializes the Flash interface and the Sys...

MMali.3 by Associate
  • 1418 Views
  • 3 replies
  • 0 kudos

The stepper/Motor/Driver Pins on the "STM32F407VG-Discover Board & How connect Driver to the Discovery board

Hi all,I have been trying to connect a microstep driver (Haydon DCM8027/55 Driver) to the my discover board, but I don't know how to hookup. I have the following board "STM32F407G-Disc1". I am not sure where the stepper motor/driver pins are located ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.