STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Having issues with using simultaneous timers

In my nucleo L432KC, I have set Timer 1 for PWM generation, Timer 15 as a timer based interrupt and Timer 2 as PWM input mode. Timer 1 and Timer 15 works well until a point. For example, I wanted a 50 kHz update event, so I set Timer 15 Precaler 0 an...

xpp07 by Senior
  • 801 Views
  • 0 replies
  • 0 kudos

STM32F105 USB HID host

I'm developing HID Host for working with standard PC keyboards.I face with problems in function USBH_HID_GetReport from cubemx, it never returns USBH_OK. Absolutly same problem explained here http://forum.easyelectronics.ru/viewtopic.php?f=35&t=23447...

urasinov by Associate II
  • 861 Views
  • 0 replies
  • 0 kudos

CAN I use USB OTG_HS with internal FS PHY and get RX DMA?

In the FS mode the reference manual state that  USB RX DMA is only available in HS mode. In MXCube it seems that I can set USB OTG HS and set internal Phy to "device only". Does this activate the RX DMA? ​It also seems to change the pins assignment o...

MSimm.15 by Associate
  • 1110 Views
  • 1 replies
  • 0 kudos

Interrupt problem

Without Interrupt signal STM32F207 print continuously.How to avoid it...void EXTI9_5_IRQHandler(void){ /* USER CODE BEGIN EXTI9_5_IRQn 0 */ /* USER CODE END EXTI9_5_IRQn 0 */   printf("\n\rInterrupt Occur\n\r"); /* USER CODE BEGIN EXTI9_5_IRQn 1 */ /...

Is USB mass storage available at STM32L152-EVAL?

I'm considering to use a STM32l1's family microcontroller at my project, so, as I will need to plug a flash drive at my device, I would like to validate my concept with a evaluation board that can do this. Does my MCU's choice seem right?Does this ev...

LFeli by Associate
  • 1227 Views
  • 1 replies
  • 0 kudos

HAL SPI transmit/receive issues

I'm trying to use the HAL SPI driver to do a basic loopback test. I fill a buffer with incrementing values, and send that out while receiving into another buffer using HAL_SPI_TransmitReceive. I have 2 separate conditions both of which show odd behav...

Konami by Senior II
  • 3828 Views
  • 4 replies
  • 0 kudos

STM32 F334R8 HRTIM Comparator Blanking Function

Hi, I have a question about connecting Comparator with HRTIM. I am currently working on Buck Converter with Digital Peak Current Mode Control. In this kind of control I need to measure the current of the inductor and compare it with another current w...

KKr�? by Associate
  • 879 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.