2018-10-16 7:26 AM
Without Interrupt signal STM32F207 print continuously.How to avoid it...
void EXTI9_5_IRQHandler(void)
{
/* USER CODE BEGIN EXTI9_5_IRQn 0 */
/* USER CODE END EXTI9_5_IRQn 0 */
printf("\n\rInterrupt Occur\n\r");
/* USER CODE BEGIN EXTI9_5_IRQn 1 */
/* USER CODE END EXTI9_5_IRQn 1 */
}
2018-10-16 8:53 AM
>> print continuously.How to avoid it...
Try clearing the interrupt source...
2018-10-16 9:04 AM
void EXTI9_5_IRQHandler(void)
{
/* USER CODE BEGIN EXTI9_5_IRQn 0 */
/* USER CODE END EXTI9_5_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_6);
/* USER CODE BEGIN EXTI9_5_IRQn 1 */
/* USER CODE END EXTI9_5_IRQn 1 */
}
==========================================================================
void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)
{
/* EXTI line interrupt detected */
if(__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)
{
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);
HAL_GPIO_EXTI_Callback(GPIO_Pin);
}
}
===========================================================================
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
if (GPIO_Pin == INTERRUPT_Pin) {
printf("\n\rInterrupt Occur\n\r");
}
}
When I use this code ,and I just placed the jumper in interrupt pin, the Interrupt get occur without any input signal.Even though I set low priority
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.