STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F767ZI and USART by HAL.

Hello,I have a strange problem with my STM32F767 ZI and USART communication.With CubeMX, I set USART2->Asyncronous, SYS->Debug Serial Wire and RCC-> HSE Active (crystal/ceramic resonator).So I generated a project for Atollic Truestudio and insertedHA...

X-NUCLEO-PLM01A1 - Doubt about this shield

Posted on February 23, 2018 at 18:14Hello people.I was studying the datasheet of Shield X-NUCLEO-PLM01A1.This Shield is intended to implement Power Line Communication on DC voltage lines.Why use two lines of cable pair for communication between the ...

Comparing Atollic with IAR - code size

I am moving a large existing project from IAR to Atollic True Studio for STM32 as an experiment. I got it to build and run without too much pain, but have noticed that the ELF file which is produced is *much* larger - more than twice the size with no...

Does CAN Masking truly mask all unwanted CAN IDs?

I'm working on the STM32F1 device and have been reading the CAN filtering and masking process. I now understand how the ID mask and filter works. I do have one question though as in certain cases I'm unsure if the filter would work 100% correctly.If ...

daithi62 by Associate II
  • 829 Views
  • 0 replies
  • 0 kudos

STM32 ADC sync with PWM

​Dear whom have expericenced STM32 MCUs (STM32F411),In my target device, ADC timing control is very important. In executing ADC in STM32 MCU,  can it be fully synchronized with PWM generated from STM32 MCU?I'd like to use PWM signal as start trigger ...

HKwon by Associate
  • 1101 Views
  • 1 replies
  • 0 kudos

HSE startup timeout on STM32F103RET7

I'm new to the STM32 so I apologize in advance for the trivial question.In the following code from SetSysClockTo72() system_stm32f10x.c, the value for HSE_STARTUP_TIMEOUT is 0x0500.  What max delay (msec) does this equate to? /* Wait till HSE is read...

DMath by Associate
  • 2344 Views
  • 1 replies
  • 0 kudos

STM32F429 shorted unexpectedly

I was working on the MCU STM32F429 while it was connected to the PCB when it shorted unexpectedly. The PCB at the time wasn't being used to power the board, or drive the motors. The Power source was my laptop and no external batteries. The USB cable ...

RDHIN by Associate
  • 1271 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.