2018-10-17 12:15 AM
Hello,
I have a strange problem with my STM32F767 ZI and USART communication.
With CubeMX, I set USART2->Asyncronous, SYS->Debug Serial Wire and RCC-> HSE Active (crystal/ceramic resonator).
So I generated a project for Atollic Truestudio and inserted
HAL_Delay(500);
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_UART_Transmit(&huart2,"Hello",5,1000);
//Toggle On board LEDSs, for testing...
HAL_GPIO_TogglePin(led2_GPIO_Port,led2_Pin);
HAL_Delay(500);
HAL_GPIO_TogglePin(led3_GPIO_Port,led3_Pin);
HAL_Delay(500);
}
/* USER CODE END 3 */After compiling (without errors) and resetting, program runs correctly (on board LEDs swith on/off) but no message to my terminal.
I connect my Nucleo to CN1 (ST-link USB port) as I do with my F4, but without success.
Serial config is OK.
Any suggest?
Thanks and best regards
2018-10-17 12:23 AM
How about working backwards ?
Next thing would be to check if there is a signal on the TX lines while sending - on both ends.
If not, the init code is probably not correct.
2018-10-17 2:08 AM
The code is quite simple, generated by CubeMX plus few lines - at first it was simply:
HAL_Delay(500);
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_UART_Transmit(&huart2,"Hello",5,1000);
}
/* USER CODE END 3 */With my STM32F446RE I haven't problems, but with F7s it doesn't work...
Is it possible there is a different approach to USB communication (F446RE has a single USB port)?
I generally use STlink USB port as a VirtualCOM and it works well (tested with speed from 9600 to 460800). As terminal I use TeraTERM, Putty and Arduino Serial Monitor.
In Debug mode, HAL_UART_Transmit instruction is processed but nothing appears on TeraTerm windows.
CubeMX set the typical stm32 PA2(TX) and PA3(RX), but F767ZI pinout doesn't refer PA2 as UART pin on CN12...
2018-10-17 2:44 AM
ops... the last part of my message was cut off...
If I connect a Logic Analizer on TX pin-CN5 (ST-Link "half board") no signal is recorded, so AvaTar is right, there is a init problem. Is it possible that ST-link TX pin isn't PA2 and I didn't understand STM schematics?
Thanks, AvaTar, for your help!
2018-10-17 8:06 AM
News about HAL_UART_Transmit(): if I connect a serial-to-USB device (a cheap SiliconLabs CP210x) to UART2 TX pin, I can view my message on terminal. So the problem isn't HAL function but it is the communication (or link) between UART2 (or UART3?) to USB CN1.
I can see "ST link Virtual Port" as in my F4, but (probably) I cannot initialize my code to use it....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.