2018-10-26 12:22 PM - edited 2023-11-20 9:33 AM
Hello Everyone,
I am using Nucleo-32 board in my project. I am programming USART to receive 10 character data and then transmit this 10 character data back.
Problem that I am observing is that if accidentally 11 character it is suppose to display error message after that every time I enter 10 character string, my response character shift right+1. Can someone
Please find below code:
HAL_Init();
SystemClock_Config();
GPIO_Toggle();
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
__HAL_RCC_USART1_CLK_ENABLE();
UartHandle.Instance = USART1;
UartHandle.Init.BaudRate = 4800;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
//UartHandle.Init.OverSampling=UART_OVERSAMPLING_16;
//UartHandle.Init.OneBitSampling=UART_ONE_BIT_SAMPLE_DISABLE;
UartHandle.Init.Mode = UART_MODE_TX_RX ;
if(HAL_UART_DeInit(&UartHandle) != HAL_OK)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
}
if(HAL_UART_Init(&UartHandle) != HAL_OK)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
}
LTC_2873();
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_7,GPIO_PIN_SET); // Mode RS485
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_14,GPIO_PIN_RESET); // RS485 Terminator Enable
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_SET); // RS485 Driver Enable
HAL_UART_Transmit_IT( &UartHandle,&aTxBuffer[0],strlen((const char*)aTxBuffer));
HAL_Delay(1000);
while(1)
{
do
{
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_RESET); // RS485 Receiver Enable
HAL_Delay(20);
while(HAL_UART_Receive_IT( &UartHandle,&aRx_Buffer[0],10)!=HAL_OK);
HAL_Delay(20);
}while(rx_cplt!=1);
HAL_Delay(50);
if(rx_cplt==1)
{
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_SET); // RS485 Driver Enable
HAL_Delay(20);
HAL_UART_Transmit_IT( &UartHandle,&aRx_Buffer[0],10);
HAL_Delay(20);
rx_cplt=0;
}//end of if
}//end of while(1)
}
2018-10-26 12:26 PM
2018-10-26 1:31 PM
you should be using the DMA functionality, it works very well and trouble free.
I cannot see where you set rx_cplt, I cannot see where you load the aRx_Buffer for transmission
not a good idea to use the same buffer for Rx and Tx...
then you are not sure which parts are Tx or Rx..
this line seems wrong, you should only turn on the RxInterrupt once...
while(HAL_UART_Receive_IT( &UartHandle,&aRx_Buffer[0],10)!=HAL_OK); <--- waiting here for HAL_OK
maybe you should change that to:
HAL_UART_Receive_IT( &UartHandle,&aRx_Buffer[0],10);
this one: change to Tx buffer
HAL_UART_Transmit_IT( &UartHandle,&aTx_Buffer[0],10);
2018-10-26 1:42 PM
1) where is rx_cplt is set? :
Answer: It is set in Rx call back function
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{
rx_cplt=1;
}
2) Change it to &aRx_Buffer[0]
Answer: I already tried it not, not very helpful
3) Why I am using same buffer for Tx and Rx
Answer: I am trying to Transmit back my received data
4) Why while(HAL_UART_Receive_IT( &UartHandle,&aRx_Buffer[0],10)!=HAL_OK);
Answer: Beacuse I want my while(1) loop- continuous loop to wait here it receives some data for futhur action
2018-10-26 1:43 PM
I will Try with DMA but I guess it will give me same results when I will enter data string more than limit
2018-10-26 1:51 PM
you must separate the Rx and Tx buffers...
then you will know what is happening.
HAL_UART_Receive_IT is set and forget... You should not be waiting on this line.
you should only wait for the Rx_Cplt flag.
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_RESET); // RS485 Receiver Enable
HAL_UART_Receive_IT( &UartHandle,&aRx_Buffer[0],10);
do
{
}while(rx_cplt!=1);
2018-10-26 2:16 PM
You were right I should not have "while(HAL_UART_Receive_IT( &UartHandle,&aRx_Buffer[0],10)!=HAL_OK);" As I using interrupt method and not polling method. Thank for that
I made a copy of array and then used that copy for Tx,
But I Still see the same issue when I send more than 10 character
2018-10-26 2:26 PM
show/zip your code... I am guessing here...
do you have a scope ?
Load TX buffer with "Text1" Transmit, receive into Rx buffer, check your text.
then
Load TX buffer with "DifferentText" Transmit, receive into Rx buffer, check your text
You should be using the DMA functionality.
2018-10-26 2:37 PM
Can you explain me this
#if defined(USART_CR1_FIFOEN)
uint32_t FifoMode; /*!< Specifies if the FIFO mode is being used.
This parameter can be a value of @ref UARTEx_FIFO_mode. */
uint16_t NbRxDataToProcess; /*!< Number of data to process during RX ISR execution */
uint16_t NbTxDataToProcess; /*!< Number of data to process during TX ISR execution */
# end if
It is part of STM32l4XX_HAL_USART.h
2018-10-26 3:07 PM
I haven't used the L4 series yet, you will have to cope with the slight differences there...
Just use the DMA, it is very good.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.