STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 VCP vs Windows 10

Posted on August 14, 2015 at 15:33Hello Guys,My product can not send data to my computer since I upgraded it from Windows 8 to Windows 10.So I have one question, meanwhile a new version of the driver is released, how can I fix this issue ? Thank you...

zaid23 by Associate II
  • 5132 Views
  • 13 replies
  • 0 kudos

hal_i2c_addrcallback not invoked with STM32H7

I'm working with STM32H743 and faced the problem that"hal_i2c_addrcallback doesn't invoked", it was invoked in other STM32 series such as F4 but H7 series doesn't work. does anyone faced same problem ? and if you have any clue ?

KKane by Associate II
  • 1499 Views
  • 2 replies
  • 0 kudos

serial driver using cmsis ?

Hello,Is there a cmsis driver for uart ? I build with stm32cubemx, but I did not find any cmsis files for any driver (I also don't see in cube anywhere we can state that we want to use cmsis driver)I also did not find it in examples of stm32cubeh7:en...

ranran by Senior II
  • 2240 Views
  • 3 replies
  • 0 kudos

PI controller using an L432KC nucleo

I'm designing an embedded PI controller using a STM32 Nucleo board. In the PWM configuration, a 0 means 0% duty and 800 means 100% duty. The objetive is to regulate the speed of a PMDC motor, i.e, to keep the RPM under load variations. I'm not sure y...

xpp07 by Senior
  • 814 Views
  • 0 replies
  • 0 kudos

USB HOST Does not read the image binaray from USB stick

HI ,I have implemented USB Host facility in my custom board which has STM32F429IG MCU , My application does detection of USB stick and reads the image binary from there , where as The functionality works as intended only with some USB sticks and also...

Vprabhu by Associate II
  • 1950 Views
  • 3 replies
  • 0 kudos

How to power a STM32F746G-DISCO board from the CN6 VIN pin ?

Hi,I'm trying to power a STM32F746G-DISCO board from the CN6 VIN pin.I have a voltage regulator that output 11VDC current.The screen turns on but the program never start and LD6 and LD3 become red after a few seconds.I measured the current between GN...

0690X000006CBPHQA4.png
NMath.8 by Associate II
  • 6052 Views
  • 16 replies
  • 0 kudos

Reading an array using STMStudio

I tracked this variable using STMStudio. See picture attached. I want to get those values to plot them in MATLAB. I tried creating an array, but STMStudio seems to have latency problems with updating a large array. How could I achieve this?

0690X000006COMnQAO.png
xpp07 by Senior
  • 693 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.