STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 qspi: reading registers

Posted on March 14, 2018 at 13:28Hello there,I am using STM32L4 series MCU and I am trying to interface with a M25Q Micron memory using QSPI. Following the examples given from ST I have noticed that there are no HAL functions allowing registers read...

How can I manage 2 SPI slaves (N°1 STPM32 and N°1 STPM34) with SPI chip select with STM32 Standard Peripheral Libraries with only a master micro ST STM32F100x8 ?

I need to use STM32 Standard Peripheral Libraries because I already use it for other Peripheral on the same board. I fine some example of stpm_metrology using HAL library, but I cannot use it!Do you have some example of SPI communication with STPM3X ...

LuxMux by Associate
  • 656 Views
  • 0 replies
  • 0 kudos

Where can I get details on how to generate SAI clocks?

I'm using an STM32F76x series and am trying to find the relevant information on the clock generation capabilities of the audio PLL.The datasheet is pretty blank and the reference manual describes the SAI clock generator but not how to generate the in...

sjalloq by Associate
  • 1326 Views
  • 2 replies
  • 0 kudos

Alternate pin selection for quadspi_ncs in STM32l476vg.

may i get any help in selecting alternate gpio pin for quadspi_ncs functionality in STM32l476vg. As per the datasheet only PE11/PB7 can be selected as quadspi_ncs. Apart from PE11/PB7 can i use any other GPIO for the same functionality.

nb by Associate
  • 918 Views
  • 1 replies
  • 0 kudos

Resolved! Generate 2 second break from UART

I'm trying to generate a 2 second break from USART1 on a STM32F105. It's needed for a custom protocol running on top of LIN: the TX line must be driven low for 2 seconds.UARTs like 8250 and 16550 have a Set Break Enable Bit (SBE) in their Line Contro...

0690X000006CO4eQAG.png

Regarding Delay

Hi..... i am a masters student from india. I have developed a code for RGBW now i want to include strobe effect for that i have give a hal_delay it is working fine now i want to change the PWM of RGBW when it is in strobe effect both has to work simu...

saiteja by Associate II
  • 2504 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.