2018-11-26 12:08 AM
Hi,
I need to perform write and read operations on an external flash memory through spi protocol.
The spi peripheral in the stm32f103 can be configured to 8 or 16 bits data frame lenght.
I would like to be able to send longer frames.
Is it a possible solution to send frames that are a multiple of 8 bits keeping the CS low between them? It will generate a communication error in the flash or are they going to be seen as a one longer spi frame?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.