STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART baud rate problem with STMF767ZI processor

​I have a UART on an STM32F767ZI  configured for 9600 baud. The baud rate of the external transmitting device is measured as 9632. I have found that the F767 is very sensitive to baud rate difference and setting the device to 9600 and 3 samples will ...

read multiple ADC channels of same ADC without DMA

hello!I want to read multiple ADC channels of the same ADC without using DMA. But I'm continuously facing some unknown issues (on ADC3 channel 12 &13's value randomly switching). So If any previously done example codes available for STM32f20X using t...

Simple "Hello World" LED blink software available?

Further:Is there some simple "Hello Word" HID USB example available for STM32H7 Nucleo? (like in STM32F4 good old discovery times ... e. g. sending some value to this USB HID Demonstrator PC software?)?How can I search in this new forum setup in the ...

flyer31 by Senior
  • 1858 Views
  • 7 replies
  • 0 kudos

Problem with TIM1 configuration of STM32F303CD

Hi, I want to configure my TIM1 to use it for driving a bldc motor. I have made several configuration in the registers, but it won't work. TIM1_CR1bits.CEN = 0; //Timer enable TIM1_CR1bits.DIR_= 0; TIM1_CR1bits.CMS = 0b01; TIM1_...

MSeib by Associate
  • 552 Views
  • 0 replies
  • 0 kudos

How to get the STM32F7 CAN peripheral out of passive mode

I have several slave devices devices hanging off connected to an STM32F7. When I power cycle the slave devices, the REC field in the ESR is greater than 128, causing the EPBF bit (in passive mode) to also be set. If I reload the chip, ESR is cleare...

NWalk by Associate
  • 766 Views
  • 1 replies
  • 0 kudos

Please give some help on L1 cache and MPU

Hello,I am working with STM32H7, Nucleo board and Atollic TrueStudio. I have a test routine processing an array of data that is in flash, test routine is also in flash. Around it I set and clear a portbit and measure execution time. Now I wanted to s...

PDR/POR reset once shortly after startup

Posting here as accidentally posted under wrong topic and was deleted...I am using an STM32F429 on a custom board. The chip is resetting once shortly after starting up, around 10 secs. I put this code at the beginning of the main function: if (__HA...

0690X000006CUuCQAW.jpg 0690X000006CUuHQAW.jpg 0690X000006CUuMQAW.jpg
hjm by Associate II
  • 919 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.