STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Discovery and MPEG4 decoding

Posted on November 10, 2013 at 07:51Is it possible to decode a mpeg4 file in stm32f407 .at least 15 fps & 320x240 pixels.till now  i can decode jpeg pics quite fast . if its possible is there any open source library to do this?i have looked at ffmpe...

Resolved! STM32F429: The FLASH_OPTCR register has been set to 0xcfffaaed and nothing is working - how can the 0xc at the start be cleared to recover the board?

Hi AllI have been experimenting with setting flash sector write protection but found that when I did I could no longer program with the debugger. I managed to reset the options by writing the unlock sequence via the debugger (that can still connect) ...

hpipon957 by Associate III
  • 1212 Views
  • 2 replies
  • 0 kudos

TIM2 exact timebase settings

Dear all,I'm using the STEVAL-PCC009V2 based on a STM32F103RBT6 microcontroller, set to work with an internal clock frequency equal to 72 MHz so CK_INT = 72 MHz (refer to figure 100 of RM0008 Rev. 19, pag. 367/1132).I need to obtain a 10 ms time base...

FF1 by Associate III
  • 4023 Views
  • 4 replies
  • 0 kudos

Resolved! What is "bus turnaround phase"?

I have basic understanding about buses, but this term is new to me.What's bus turnaround phase - and measured from where to where?Google hasn't been my friend on this.

Resolved! STM32L1 SPI DMA Receive half duplex (no HAL, only LL)

Hi All, My environment: STM32L151CB, SPI2 Master, DMA1 Chan4(RX) and Chan5(TX)I moved from HAL to LL (to save memory) and faced with the following issue:When I configure SPI to receive data by DMA and setup only RX DMA channel SPI transaction doesn't...

Connect STM32L4xx with S2868A1

Hi, everyone.I want to connect a STM32L475RG board with an extended board, more exactlyS2868A1, which comunicated on SPI protocol. More that, i want to connect these 2 components with another Stm32L4 and S2868a1, and comunicate with them via S2-LP mo...

cionu by Associate
  • 723 Views
  • 0 replies
  • 0 kudos

STM32H7 Ultra slow RAM access time of 500kHz

Hello, I am working on developing board where STM32H7 will talk via SRAM interface to FPGA and i hit the problem.I use IAR ARM and H743I-EVAL SRAM example, and guess what, if i make simple loop with just single write to SRAM like this, I only get 50...

Linas L by Senior II
  • 1882 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.