STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

To wich parameter refers HSE oscillator characteristic Gm in STM32L443 datasheet on page 123? Does it refer to AN2867 parameter gm or to Gm_crit_max?

I'm in doubt about the transconductance parameter of the HSE oscillator in STM32L443.To select an appropriate cristal I studied AN2867.If the datasheet of STM32L443 which notes "Gm = 1.5mA/V" refers to gm the transconductance of the passive elements ...

ChrisK1 by Associate II
  • 1442 Views
  • 1 replies
  • 0 kudos

STM32F407IGT6 ADC Input Range

Hello,Am using STM32F407IGT6 in my design. I power the VDD, VDDA & VBAT from 3.3V.I use an external voltage reference using LM4121AIM5-ADJ which generates 3V from 3.3V input.When I use this external reference of 3V as VREF+, I would like to understan...

SK.7 by Associate
  • 1597 Views
  • 2 replies
  • 0 kudos

How to print logs for B-L475E-IOT01 board ?

I am using STM32CubeMx to generate default files to build with Makefile. I edited the main.c to print some logs using printf. I am unable to see the same logs in the serial. Am I missing anything ?

KVenk.2 by Associate II
  • 1360 Views
  • 2 replies
  • 0 kudos

Resolved! HSE fails to initialize in STM32F205ZG using SPL

hello!  I was devolving my project on the "STM3220xG eval-board" (based on controller "STM32F207IGH6"). Now as my custom made controller board is ready (based on "STM32F205ZGT6"), I ported my code for it by changing in peripheral's Pin-numbers and Ke...

How to calculate the prescaler of TIM?

Posted on September 28, 2017 at 06:50HI.Now I'm trying to implement TIM into the STM32F429i-DISCO kit.But I need to help how to calculate the prescaler and period value for user?As I know currently I used 180Mhz as system clock. and I want to set TI...

0690X00000608QBQAY.png

Android USB HID driver for STM32F1 Series

Hello there.  I am trying to implement a USB HID driver for the STM32F1 series.  I tried several generic examples of Android USB HID drivers on the web, but none of them seem to work with what we have.  I was wondering, how would I approach implement...

How to debug properly UART interrupts?

My UART works well in normal mode, but when I want to analyze callbacks for Rx in debug mode it doesn't work properly. I mean when I set breakpoint at HAL_UART_RxCpltCallback and I'will send bytes from terminal, debugger stops at this callback and do...

BHowa by Associate
  • 2310 Views
  • 2 replies
  • 0 kudos

STM32L476 CAN Bootloader

Hi,we want to use the built-in CAN bootloader of a STM32L476. We experienced some strange behaviour while testing with a nucleo board, which we could partly fix.First of all, after a write command, sometimes two ACK are sent, the data is also written...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.