STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using nucleo board as offline programmer

Hi,i'm wondering if there is an easy solution for using nucle board as field programmer over SWD interface. I would like to programm blank stm32 device directly from nucleo board using external flash or stm32 device content. It should be done over on...

DCMI to QSPI storage

Hi there,I am trying to use DCMI on STM32F469. Due to the limitation of the internal RAM, external RAM is needed. One option is to incorporate a QSPI-PSRAM. After reading "AN5020 - Digital camera interface for MCUs", my question still remains: Can DC...

alexP by Associate
  • 1300 Views
  • 2 replies
  • 0 kudos

SPI slave configuration

Hi to all,I'm dealing with SPI interface in slave mode and I am experience some problem in communication.I am using a ST32F030 MCU and I enabled RXNEIE interrupt for receiving data. Hereafter is the code:CONFIGURATIONRCC->APB2ENR |= RCC_APB2ENR_SPI1E...

Issue with f_write function (STM32F769I EVAL)

Hello everyone,I have a problem with my code. I'm trying to write a program to take picture from camera and save it as motion jpeg video (MJPEG) in to USB. I build already the header and the structure of MJPEG file but it's really weird when I try to...

0690X000006CXbrQAG.png

STM32F4 -

Posted on June 03, 2016 at 00:09Hisorry that's just a typing mistake :)

eittinfo by Associate II
  • 2239 Views
  • 5 replies
  • 0 kudos

STM32F407 FLASH erase fail with IWDG enabled (HAL)

Posted on May 15, 2017 at 12:47Hi,I am having a problem writing to flash with the IWDG enabled, presumably I am missing something.I have cut my project down to a minimum that reproduces the problem.The program initialises the HAL and system clocks a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.