2018-12-03 2:22 AM
If I want to use the SafeRTOS for critical issue can I use it in the cubeMX as I use today the FreeRTOS?
If it is possible or not at this stage, and if yes what adaptation do I need to do to use it?
Is there any guide for immigrate Safe RTOS to CUBEMX?
Regards
Bar.
2018-12-03 5:17 AM
I'd say no.
SafeRTOS is a pre-certified product by Wittenstein, and not freeware.
Licence costs use to be in the 5/6 digit figure range.
> Is there any guide for immigrate Safe RTOS to CUBEMX?
Probably possible, but sounds to me like implanting a Rolls-Royce engine into a golf buggy.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.