STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI TX DMA not work after mcu power on

Hi All,I use STM32f103C8T6 mcu to control a 5" TFT (480x272) display in direct mode.TIM1 PWM is the 9Mhz pixel clock,TIM2 is the column counter,TIM3 is the row counterand TIM2 channel 2 in compare mode, start SPI DMA transmit once in lineso, the SPI ...

ExtSol by Associate II
  • 1360 Views
  • 2 replies
  • 0 kudos

STM32F4DIS-BB + ETH + CubeMX

Posted on April 25, 2014 at 12:56Created a project targeting STM32F4DISCOVERY + STM32F4DIS-BB from a scratch with CubeMX. Managed to blink LEDs and send bytes over UART but now struggling with Ethernet and LwIP. I have referenced STM32F4DIS-BB examp...

jarno by Associate III
  • 8494 Views
  • 11 replies
  • 1 kudos

Disable FSMC in Stop mode

Posted on July 11, 2017 at 09:32Hi,I'm using Stop mode on a custom board with STM32F207. There is a SRAM on the board for data storage.I turn off SRAM in Stop mode, to reduce power consumption. Now I want to disable the FSMC of SRAM too. Therefore I...

SRAM scattered architecture on the STM32H7

Hello For the STM32H7 micro controllers what does a "SRAM with scattered architecture mean". "The STM32H7x3 line provides from 1 to 2 Mbytes of Flash memory, 1 Mbyte of SRAM with a scattered architecture: 192 Kbytes of TCM RAM (including 64 Kbytes of...

Resolved! Can't enable PLL properly for STM32F767

Hi,I'm having a hard time configuring the system clock. It seems that I'm achieving 16MHz, but I want to run at full speed (216MHz). From what I'm seeing, the problem is that the System Clock Switch isn't changing to PLL. If I try to change bits 1:0 ...

Recently I bought original NUCLEOF103RB development board. 1.Is there any inbuilt serial window available in KEIL IDE ?. 2.Can I check serial output through the same USB port while debugging (Like Arduino) ?

I am new to this controller, Before I am well aware of PIC and Atmel chips, Now I would like to move to 32 ARM that is why I am choosing this developments board. This compiler is very new for me compared with CCSC PIC and Arduino, So please tell me w...

Nucleo-STM32F4 compiling error using Eclipse

I just bought a Nucleo-STM32F466RE and have a problem to use it. I tried to use Eclipse like this tutorial: https://www.carminenoviello.com/2014/12/28/setting-gcceclipse-toolchain-stm32nucleo-part-1/ and I have a problem in compiling the test project...

JJuli by Associate
  • 707 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.