2017-07-11 12:32 AM
Hi,
I'm using Stop mode on a custom board with STM32F207. There is a SRAM on the board for data storage.
I turn off SRAM in Stop mode, to reduce power consumption. Now I want to disable the FSMC of SRAM too. Therefore I use the function HAL_SRAM_DeInit before entering Stop mode. After leaving the Stop mode I reinitialize the FSMC by using HAL_SRAM_Init.
After reinitialization the FSMC doesn’t work correctly and I can’t access SRAM.
Is there a different way to disable FSMC?
Thanks in advance
Guenter
2018-12-09 6:17 AM
Hi Guenter,
Is it solved ? I have similar needs.
by the way, If you stop external sram (FSMC), isn't it problematic for your application ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.