STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-VS4A -- How to pass Amazon ATS certificates?

1.Uncommenting one line in service_asset.c still can't work.Request a token from Amazon website. It shows token "ANeQCyBUgoyAFxrpfsUJ" in browser. But my STM32F769I shows below messages: Always can't pass Amazon ATS certificates.=====================...

jesson by Associate II
  • 4629 Views
  • 9 replies
  • 1 kudos

Error Handler

If i remove while(1){} from Error handler and Hard fault handler is there any chance of it to effect micro controller

saiteja by Associate II
  • 2114 Views
  • 5 replies
  • 0 kudos

STM32F411 I2C DMA FUNCTION QUESTION

I'm using STM32F411RCT chip and using I2C3 slave is BMP280 * 2ea and HDC1080​​The bmp280 is implemented as a function of HAL_I2C_Mem_Read.HDC1080 is implemented as a function of HAL_I2C_Master_Transmit & HAL_I2C_Master_Receivenow, I change this fun...

mkim.51 by Associate II
  • 965 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L433: can't make sense of Flash Loader Demonstrator

During development I've been using ST-LInk to program the STM32L433 which of course works perfectly. I want to release the firmware and allow users to be able to update the code over UART2. I've set BOOT0 and can see the device using the latest versi...

Resolved! Do a corralation with DSP Library

I have a 32F746GDISCOVERY and would like to test the dsp functionalities with a correlation.I have the following code:#include "arm_math.h" extern void arm_correlate_fast_q31(q31_t * pSrcA, uint32_t srcALen, q31_t * pSrcB, uint32_t srcBLen, q31_t * p...

MMett by Associate III
  • 2138 Views
  • 2 replies
  • 0 kudos

STM32F429I-DISCO - USART3 outputs only 1.6V

Hi everyone,I am trying to get USART3 running on my STM32F429I-DISCO board. USART3 is configured with the following configurations:Mode: AsynchronousHardware Flow Control: DisableBaudrate: 115200, Word Length: 8, Stop Bits: 1GPIO: PD8 = TX, PD9 = RXI...

smrtkai by Senior
  • 2316 Views
  • 4 replies
  • 0 kudos

stm32f722ZE Nucleo UART sample code problem

Posted on January 10, 2018 at 21:56Hello, I've just built the UART sample code for the 722ze Nucleo board and have a problem. I have not modified the code (except for the transmitted character buffer).  The sample code shows setting up the unit for ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.