STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why low the GPIO output speed?

Dear ST Community,The MCU type is: STM32F407VGT6I try to write GPIOx->ODR register with DMA2. The trigger signal is TIM1 update event. I set the timer period frequency is 9Mhz and i measure 4.429Mhz on GPIO pin. Why?here is my code:#include "stm32f4x...

ExtSol by Associate II
  • 1269 Views
  • 2 replies
  • 0 kudos

Understanding of NOLOAD directive for GNU-LD

Hi everyone,I want to have a section in FLASH that will act as an EEPROM with some initial values defined at compile time. I have defined the section in the linker script (the last page of the FLASH) and I can see it in the .map file correctly.Howeve...

Kraal by Lead
  • 3914 Views
  • 2 replies
  • 0 kudos

STM32L051 voltage regulator in Stop mode

Hi,Turning Voltage regulator into low-power mode (LPR) in Stop mode possible only for Category 1 devices as stated in RefMan (6.4.1 p158), but referring on datasheet for L051 family (that's category 3) that's however possible (3.1 p14 & 3.4.3 p21). S...

MZubk by Associate
  • 768 Views
  • 0 replies
  • 0 kudos

A patch for USB HOST Library Bug

Posted on January 27, 2012 at 20:58 There is bug in USB Host library that causes to wrongbehavior if the attached device has more that one interface. EP properties for interface 0 is overriding by the values for next interfaces. There is also a ...

dzuikov by Associate II
  • 1643 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F0xx BxCAN Loop-back Transfer Delay

Hi,I am working on STM32F042.I have setup the BxCAN peripheral into loop-back silent mode, and it works fine. I can transfer and receive every single frame I am transmitting and no error conditions are detected.However, I have noticed that when I wan...

MArgi by Associate II
  • 1191 Views
  • 1 replies
  • 0 kudos

HAL bug in LPTIM interrupt.

Posted on November 27, 2017 at 14:20Hi everyone,I'm trying to clear my head around interrupts with an STM32l0x3. I'm not using HAL functions, rather I'm trying to understand the logic behind all this.This becomes a little bit messier since the NVIC ...

0690X00000608xyQAA.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.