STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 CAN-FD using CAN 2.0 transceivers.

Posted on May 04, 2018 at 00:04Hi,   I'm thinking in replace  a STM32F7 with a STM32H7 on two board that has normal CAN-2.0 transceivers. I would like to know if it will work for CAN-FD frames, keeping the baud below 1 Mbps. Ari.

Asantos by Senior
  • 2760 Views
  • 3 replies
  • 0 kudos

How to use DCMI on STM32F769I Discovery board?

Title pretty much says it all. According p. 21 in the DCMI information document (link at bottom), the board supports the interface, and I'm supposed to connect the camera through the GPIO pins. But I've found no mention of how to do this in the board...

ukn by Associate
  • 2209 Views
  • 3 replies
  • 0 kudos

USB OTG host multi-application.

Hi , I have an application that streams multiple audio sources over USB device Audio class to PC. The PC detects audio device and the streams work.I'm building hardware based on X-CUBE-MEMSMIC1 and don't want to use a second micro ( st-link ((stm32f0...

benyBoy by Associate II
  • 1333 Views
  • 1 replies
  • 0 kudos

usb bootloader

Hi(All?) my nucleo board(s) is/are detected as a USB device in windows. I can drag and drop a firmware binary on them. And the Firmware is automatically updated after power cycling the board. I want to design my own board and use the USB to update t...

PWM on TIM1 CH1 of NUCLEO--F303RE does not start

Hello,I dont't know why in my projetc the PWM daoes not start.I would generate a PWM with Duty =50% and Period =10msec. I use a NUCLEO--F303RE.I started with CubeMX to generate the project configuring IO (blinking the green LED) and the PWM on TIM1 C...

MCere by Associate
  • 2927 Views
  • 5 replies
  • 0 kudos

Nucleo l476RG. Reset when connect to laptopusing usb

Hello.I have a nucleo powered with external 5V. I use to log info using usb.Eache time i need to talke a log to the log, i cannoct my laptop and MCU reset.Anyone know if i can hovoid this? Remove SB12 could help Me? any other hint?Regards,Carmelo

stm32f4 by Associate II
  • 2705 Views
  • 5 replies
  • 0 kudos

Why do GP14 and PB15 GPIOS not work for me?

All other GPIOS work but these two do not. They get the same voltage as the rest (0 and 3.2V). All pins Vdd and Vss I have them well except pin 97 VDD_USB that by mistake I have connected to GND.I have attached the project with which I have been test...

FFran by Associate II
  • 2062 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.