2018-12-11 6:54 AM
Hello
i want to exit from STOP mode using RTC has in the example of STM32Cube\Repository\STM32Cube_FW_L4_V1.12.0\Projects\NUCLEO-L476RG\Examples\PWR
But the STM32 exits immediatly after the WFI execution.
It works well with the HAL_PWR_EnterSTANDBYMode function (a reset from RTC occurs 10s after WFI execution)
here's the code :
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
//0.5ms*20000=10s
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 20000, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
HAL_SuspendTick();
HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);
SYSCLKConfig_STOP(); //re-start the ticks !!!
HAL_ResumeTick();
Have you any idea ?
thanks
Regards
2018-12-17 4:44 AM
Hello,
Do you have another wake up source enabled ?
Regards,
Mohamed Aymen.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.