STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! InvalidateDCache with AXI-SRAM gives HardFault

Hello,I have recently moved RAM from DTCM to AXI SRAM (so that I get more RAM).It then failed in dma example.After investigation I found out that the call to  SCB_InvalidateDCache results in HardFault_Handler.I've changed it to use   SCB_Invalida...

ranran by Senior II
  • 2376 Views
  • 3 replies
  • 0 kudos

Bootloader in STM32L0

Posted on February 19, 2015 at 10:57Hi all,Is it necesary to implement a additional code in my application to jump to the bootloader? #magic-eight-ball

gerardo by Associate II
  • 2587 Views
  • 5 replies
  • 0 kudos

HAL_NVIC_SystemReset() is not consistent

In my STM32L432 project (Keil) I need to use a system reset.System should be able to reset by external command, and it's also used in bootloader<->application jumps. I am using HAL_NVIC_SystemReset() for this purpose. I've noticed that once in a whil...

Dual Bank Flash

HelloI would like to know if all STM32 cards have dual bank flash mode.I have two cards, a STM32F746 Discovery and a STM32L475 Discovery. Apparently the STM32L475 has mode but not the STM32F746.Is that right?If a card does not have a mode, is there a...

Bfren.9 by Associate II
  • 1364 Views
  • 1 replies
  • 0 kudos

Multi-Channel ADC and I2C

I'm using an IMU 9250 (who works with I2C) and I need use at least 4 ADC single-ended channels. but, unfortunately, I'm not able to accomplish it. When the STM32f303k8 has the code (i2c + 4 channel ADC with DMA) and the 4 ADC pins are not physically ...

Why is this code not being able to change the default SPI value of 0 to 1, and also the bit shift on timer is not working

#define SPI2_CR2 *(__IO uint32 *)0x40003800#define timer4_CR2 *(__IO uint32 *)0x40000800void setup() { Serial.begin(115200);}void loop() { Serial.println("SPI"); Serial.println(SPI2_CR2,BIN); SPI2_CR2=SPI2_CR2|(1<<0); Serial.println(SPI2_CR2,BIN); Se...

AHald by Associate
  • 1137 Views
  • 3 replies
  • 0 kudos

How to find start address of NOR/SRAM/PSRAM bank ?

Hello,I have created with stm32cubeMX full configuration for my project.I have 3 memories:nor flashSRAMFPGAI also find the following information in my cubemx project:Chip Select:NE1 Memory type:NOR Flash Address:24 bits Data:16 bits Wait:Asyn...

ranran by Senior II
  • 1132 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.