2019-01-21 11:02 PM
Hello,
I have created with stm32cubeMX full configuration for my project.
I have 3 memories:
I also find the following information in my cubemx project:
Chip Select:NE1
Memory type:NOR Flash
Address:24 bits
Data:16 bits
Wait:Asynchronous
NOR Flash/PSRAM/SRAM/ROM/LCD 2
Chip Select:NE3
Memory type:SRAM
Address:20 bits
Data:16 bits
NOR Flash/PSRAM/SRAM/ROM/LCD 3
Chip Select:NE2
Memory type:PSRAM
Address:24 bits
Data:16 bits
Clock:Burst Read Write
Address valid: SetBut After generating code, I can't find start address of the memories.
According to RM:
0x6C000000 -0x6FFFFFFF FMC NOR/PSRAM/SRAM 4 Bank1 (or remap of FMC SDRAM Bank1)
0x68000000 -0x6BFFFFFF FMC NOR/PSRAM/SRAM 3 Bank1 (or remap of FMC SDRAM Bank1)
0x64000000 -0x67FFFFFF FMC NOR/PSRAM/SRAM 2 Bank1 (or remap of FMC SDRAM Bank1)
0x60000000 -0x63FFFFFF FMC NOR/PSRAM/SRAM 1 Bank1 (or remap of FMC SDRAM Bank1)But why in columns above it shows "BANK1" ? (and not bank2, bank3) ?
So, which address correspond to BANK2 and BANK3 ?
Attached the project test.ico (using 4.27 cubemx)
https://drive.google.com/file/d/1n-OvGtiwXAdurKw2XfC-ZL8ysACitrhq/view?usp=sharing
Thank you,
ran
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.