STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART Frequency?

How can i change the Frequency/Speed by which the Data is transfered to the UART TX pin?

arduo by Senior
  • 1376 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4 - DAC triggering using timer example

Hi, guys. I'm using the STM32L4 discovery (MB1184C) board to test DAC (Pin PA5).I use Keil uVision 5 to debug the code.I noticed the Timer trigger option and I want to use this.I want to put this MCU to sleep at the main function's while loop.Periodi...

0690X000006DGbjQAG.png
Matthew K by Associate II
  • 2100 Views
  • 1 replies
  • 0 kudos

FORTH Compiler for STM32 devices

Posted on October 29, 2015 at 10:36If you want a development system on chip, incremental software updates, test driven interactive developments this is worth a look: Mecrisp Stellaris Forth compiler updated with support for a number of STM32 control...

jjonethal by Associate II
  • 10115 Views
  • 16 replies
  • 0 kudos

Hi, I am implementing the bank switching logic for STM32L476 Environment: Eclipse for code development : ST-Link/V2 Debugger for flashing and debugging binaries: Why below code gets stuck at the HAL_FLASH_OB_Launch(); ?

   FLASH_OBProgramInitTypeDef   OBInit;   /* Set BFB2 bit to enable boot from Flash Bank2 */   /* Allow Access to Flash control registers and user Flash */   HAL_FLASH_Unlock();   /* Clear OPTVERR bit set on virgin samples */   __HAL_FLASH_CLEAR_FLAG...

Neel by Associate III
  • 785 Views
  • 0 replies
  • 0 kudos

Resolved! ADC1 and 2 timing longer than data sheet values

Hello,I try to setup ADC1 and ADC2, but I don't get the timing values given in reference manual and data sheet. I work with STM32H743 NucleoI have setup RCC to clk ADC with 36 MHz from PLL2P. I checked the frequency at master clock out 2 on PC9. To i...

Resolved! How to get the output of the DAC full zero voltage?

Good day. Faced such a situation. I want to get at the output of the DAC zero level (writing to the register is trivially 0). That's just absolute zero does not work, on the output of the microcontroller there is somewhere around 70mV. The influence ...

evilbob by Associate II
  • 4163 Views
  • 5 replies
  • 0 kudos

STM32F334 HRTIM power consumption

The data sheet says 324.2 µA/MHz. If we take that at face value, this means a whopping 46mA at the maximal 144MHz. Is that really true? It seems a tad disproportionate.I'd be interested in an approximate breakdown of the currents: DLL "base" current ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.