STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How is make run program from ram

Hi ​every body.I need to make change some external program.In external spi flash ​i want write meny programs, and one selected program must copy to ram in fixed start address for call from main program like shift program.

MMykh by Associate II
  • 3797 Views
  • 10 replies
  • 0 kudos

STM32 Nucleo-64を使�?��?�STEVAL-STLKT01V1�?�ファームウェアを書�??�?��?��?��?� I want to change firmware of STEVAL-STLKT01V1 with STM32 Nucleo-64.

�?�?�ST社�?�ん�?�STEVAL-STLKT01V1�?�STM32 Nucleo-64を購入�?��?��?��?�。 STEVAL-STLKT01V1�?�電池を長�?�?��?��?�る�?��?�?�ファームウェア�?�書�??�?��?�を考�?��?��?�り�?��?�。 �?��?��?��?書�??�?��?��?�方法�?��?�?�り�?��?�ん。 STEVAL-STLKT01V1�?�メインプログラムも�?��?��?��?�る�?��?��?�?�り�?��...

RNish by Associate
  • 721 Views
  • 0 replies
  • 0 kudos

NSS pin (chip select) driven by hardware.

Good morning.I'm trying to use SPI communication on STM32L051 MCU but experiencing some problems. In my application, the MCU is working as a master and using all communications signals: SCK, MISO, MOSI and NSS.I started with the example code "01_Full...

LOliv by Associate II
  • 4955 Views
  • 1 replies
  • 0 kudos

STM32F429ZIT SDRAM to SPI using DMA

Hello,I'm facing a problem with the DMA and FMC. This is my setup:I'm using a STM32F429ZIT at 180MHz. I am using the same SDRAM as the STM32F429-DISCOVERY board. For the HAL configuration, I am using the STM32CubeMX software, version 4.25. This is wh...

Mvan.13 by Associate II
  • 4068 Views
  • 7 replies
  • 0 kudos

Need .SVD file to debug STM32F413ZH with Segger's Ozone

HelloI prefer to use Ozone debugger of Segger over Atollic. The only issue i have is missing of Peripheral Registers Window. In the User Manual Segger apply Ozon's users to vendors for a specific .SVD file that will allow to see Peripherals in the Re...

Yevpator by Associate III
  • 2252 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.