STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F746G-DISCO LTDC & display without HSYNC and VSYNC

Hi all, we are designing a new PCB and we would like to use an LCD that does not have HSYNC and VSYNC signals... is this possible ?The lcd is a Winstar model WF70HTIAGDNT0 https://www.winstar.com.tw/it/products/tft-lcd/module/7_0-tft-lcd.htmlThanks...

iw2lsi by Associate III
  • 763 Views
  • 0 replies
  • 0 kudos

X-NUCLEO-IDB05A1 with STM32F4-DISCOVERY

Posted on January 08, 2018 at 14:35Hi,I'm trying to port (use) X-NUCLEO-IDB05A1 board with STM32F4-DISCOVERY.I've begun developing this project by modifying SensorDemo for Nucleo-L053R8 board.I'm using Keil-MDK v5.25 (Lite). STM32F4 project is build...

Resolved! STM32F103C8Tx can tx voltage too low and can clock speed

I am using truestudio and cubemx with STM32F103C8T6. I am trying to use canbus. If I connect the cantx and canrx pins on A12 and A11 (as shown in attached cubemx file), I get an output that looks like a can frame, but has peak voltage of 400mV.cubemx...

SThre by Associate II
  • 1327 Views
  • 1 replies
  • 0 kudos

PWM dithering

I am using STM32F103C8 controller for my product desgin. I want to implement PWM dithering concept to increase my PWM resolution. after reading application note AN4507 following are my doubtswhat is meant by 1-LSB duty cycle managementOn page no 12. ...

MMitt.7 by Associate
  • 2735 Views
  • 4 replies
  • 0 kudos

Can we use the STMCUBEExpansion ble1 for stm32f407vg

HiActuelly i have a stm32f407vg connected to a SPBTLE-RF via SPI, i wanted to know if i can use the STMCubeExpansion ble1 developped on the nucleo for the stm32f407 vg ?if not, IS there an existing code for stm32f407vg ?

tTAGN by Associate
  • 756 Views
  • 0 replies
  • 0 kudos

STM32F105 I2C clock streaching

Hi,We are working with the STM32F105 chip and we want to use its I2C interface to communicate with a chip that demanding an I2C master that allows the clock stretching. We need to know if it is possible to enable this feature in the STM32F105 and how...

CAlon by Associate
  • 1187 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.