STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F3 PGA stability with low voltage signals

Hi,I am trying to use all the 4 PGAs in the STM32F303 to amplify and measure some low voltage signals (100-200mV with a gain of 8 or 16) coming from a temperature sensor. Doing so on one channel works fine, and I am able to get accurate readings once...

JThev by Associate II
  • 1328 Views
  • 1 replies
  • 0 kudos

STM32F4-DISCOVERY I2C hanging problem

Hi everyone, I have a strange behavior with STM32F4-DISCOVERY I2C communication.My system includes an STM32F4-DISCOVERY, a BLDC motor, a flow sensor (SDP601), and a pressure sensor (MS5525DSO). The motor works as a blower and 2 sensors measure the fl...

0690X000006DkTxQAK.jpg 0690X000006DkU2QAK.jpg 0690X000006DkU7QAK.jpg
QDang by Associate
  • 1706 Views
  • 2 replies
  • 0 kudos

IrDA compliant library

Posted on May 09, 2012 at 00:56One of the areas I'm looking at with the STM32 is being able to transfer files (or at least data) from an IrDA dongle from Windows to the STM32. However, as I understand it, the STM32 only implements the PHY layer usin...

shotaro by Associate II
  • 1163 Views
  • 1 replies
  • 0 kudos

LPTIM ARRM and CMPM Update Times

Posted on April 17, 2017 at 19:54I am looking for the max and typical update times for the LPTIMx_CMP and LPTIMx_ARR registers on an STM32L4x. I don't see these listed in the reference manual anywhere. Additionally, are there any settings or device ...

Parallel flash operations on STM32H743

There are multiple references in the documentation that allude to being able to do two flash operations in parallel on the STM32H743 as long as you are doing these operations on different banks.For example, the reference manual RM0433 Section 3.2 sta...

ST User by Associate III
  • 2043 Views
  • 3 replies
  • 0 kudos

Stm32f103 ir transmitter

Hi,I want to realize ir transmitter with pwm signal but i do not understand the basic principle of pwm ir transmitter. What is the right way for creating ir transmit signal with pwm? Which peripherals must be used for this( pwm, timer interrupts...?)

er3481 by Senior
  • 769 Views
  • 0 replies
  • 0 kudos

reading multiple adc channels, no dma

Posted on January 26, 2015 at 11:58 Hello List, I,m struggling with reading, without DMA, from multiple channels. Every, say, 10 msec I call: var1 = Get_ADC_Value(11); var2 = Get_ADC_Value(12); Both variables ALWAYS get ...

Sietse by Associate III
  • 4005 Views
  • 7 replies
  • 0 kudos

Memory requirements for STM32H743XI EVAL board.

Hi All,I'm trying to implement the eval board for a project seems like they have used a lot of different types of memory from HW perspective. I wanted to know what memory is being used for what purpose for this specific board so that I can change it ...

BBV by Associate II
  • 3115 Views
  • 6 replies
  • 0 kudos

Resolved! What's minimal possible jitter when using STM32 DAC with DMA?

Hi,I need to generate a special waveform via DAC on a STM32F446. DAC samples must be generated at about 240kHz but with minimal jitter. A DMA channel with timer trigger will provide the data from internal RAM or flash. What best case - minimal - jit...

MFuch by Associate
  • 2436 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.