STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 programming service

Hello everyone.I'd like to ask about the possibility of purchasing pre-programmed STM32 parts with our application.For now, we expect a low volume production in the mid term, but it is expected to grow around 1 year after product launch.Is it possibl...

jose_1. by Associate
  • 2868 Views
  • 6 replies
  • 0 kudos

STM32L071 VREFINT_DIV

Hello, my work mate made a design where we have to measure a low voltage in a smaller range (0-.120mV) on an Input.His assumption and hardware realization to meet the requirements based on datasheet DS10690 Rev 6. Here on page 63 you can find the ta...

Artur1 by Associate II
  • 1928 Views
  • 2 replies
  • 0 kudos

Problem saving data in flash memory.

Hello, guys!I have problem saving data in STM32L0's flash memory.If I save the data twice in the same location it works fine.If I save the data once CRC check fails - data writing goes wrong?!I have attached my code.Sorry for the "magic" numbers in t...

LMehm by Associate III
  • 5243 Views
  • 10 replies
  • 0 kudos

Mipi dsi with LCD issue

Hi Everybody,I have a difficult problem. I use STM32F469I-Disco to porting new LCD on it.My LCD driver IC are ILI9806E and ST7701s. they are having the same problem.they can be lighted on, but image is not the same as my setting.Example: I use BSP_LC...

CYong by Associate II
  • 3506 Views
  • 5 replies
  • 0 kudos

How to use VSP on Nucleo STM32F746 board

I have a nucleo F746 board powered from CN1 (USB from the ST-LINK side) and I am interested to use the other USB port (CN13) configured as Virtual Serial Port (VSP) and start debugging with the printf () and log on a PC (the STM32 does not yet have ...

BMM by Associate
  • 786 Views
  • 0 replies
  • 0 kudos

How do I generate 'N' PWM pulses on TIM2 CH4.

I have inherited a PCBA that needs to generate a fixed number of PWM pulses on TIM2 CH4.I have successfully setup TIM1 as the Master (with repetition count = 0) and TIM4 as a Gated Slave.TIM1 CH1 is generating 2kHz PWM indefinitely.TIM2 CH4 is genera...

CStas by Associate
  • 1371 Views
  • 3 replies
  • 0 kudos

Resolved! VCAP layout

I'm sure everyone else has noticed how the two pins to VCAP seem to be placed just over a complete side of the package away so there is bound to be some resistance/inductance in the tracking. I was wondering if anybody has ever hit problems with thi...

MikeDB by Lead
  • 1587 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.