STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743II SPI+DMA malfunction

I am porting a firmware from STM32F2/F4 to a H7 (STM32H743IIT6) platform on a custom board. There is an SST26VF064B-104I/SM flash on the boards with custom drivers with FAT FS file system driven by SPI and DMA. It works perfectly on older boards sinc...

laszpar by Associate II
  • 4435 Views
  • 8 replies
  • 1 kudos

STM32L151xx LQFP100 VDDA VREF range

Reference manual RM00385.1.1 Independent A/D and DAC converter supply and reference voltageOn BGA 64-pin and all packages with 100 pins or moreI need a bit of clarification on correct voltage ranges for VDDA and VREF+:2.4 V ≤ VREF+ = VDDADoes it mean...

Cannot find STM32L010 Keil Packs

Hi,I am receiving the STM32L010 NUCLEO board tomorrow and was trying to set up my dev environment. However, I cannot find the STM32L010 in the Keil Pack Installer.Error Message: "Cannot select device(STM32L010RBTx:STMicroelectronics), Device not foun...

BAndr by Associate
  • 1631 Views
  • 2 replies
  • 0 kudos

Resolved! Most effective way to generate waveform?

Need to generate a repeating waveform with external SPI 16-bit DAC.Using a table of values in memory, repeatedly loop through table outputting values to DAC.Delay between outputs is constant. No glitches at repeat!DMA only (no interrupts).What's the ...

How to send and receive message through UART interrupt or DMA?

< What I want to do? >Send string messages(AT command) from STM32 microcontroller to LTE module through UART, receive the reply, and store the received data in a string variable. I tried HAL_UART_Receive function and it works. However, it doesn't com...

YFuku.3 by Associate III
  • 13123 Views
  • 17 replies
  • 1 kudos

Receiving and storing the sample values

I am using the STM32F4 Board and Wolfson pi audio card for my problem, which I stated down. I am trying to pass my own sample values to the DAC, then passing out them through the speaker. Then I want to capture/sense those values (emitted signals fro...

rrach by Associate II
  • 1429 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.