2019-03-10 7:49 AM
hi i'm reviewing rm0008 ref manual for stm32f103 the adc.
accordingly, adc clock max is 14mhz and it takes 14 adc clock cycles for 1 conversion - hence 1msps per ADC.
however, from the RCC section the available prescalers are 2, 4, 6, 8
and if we take 72mhz / 6 that gives 12 mhz
and if we assume it still takes 14 adc clock cycles per conversion, that gives
1m x 12 / 14 ~ 857ksps per adc?
does it still takes 14 adc clock cycles per conversion if the adc clock runs at 12mhz?
in addition, it seemed there isn't really a feasible way to achieve 14mhz on the adc clock ?
thanks
Solved! Go to Solution.
2019-03-10 8:18 AM
>>in addition, it seemed there isn't really a feasible way to achieve 14mhz on the adc clock ?
You clock the F1 at 56 MHz?
2019-03-10 8:18 AM
>>in addition, it seemed there isn't really a feasible way to achieve 14mhz on the adc clock ?
You clock the F1 at 56 MHz?
2019-03-10 8:24 AM
i see, unfortunately if the F1 is clocked at 56 mhz, usb may not work, as 72 mhz x 2/3 (prescalers) = 48 mhz which is needed by usb.
it seemed this could be a compromise of sorts
thanks for the cool and quick response. i'd make do with 12mhz on the adc clocks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.