STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART in Synchronous Slave Mode with Interrupt not working

Hi all,I try to install a synchronous USART communication between 2 x STM32H743, one is the (transmitting only ) Master the other is the (receiving only) Slave. When transferring data via Polling everything seems to work well.But when using HAL_USART...

GS1 by Senior III
  • 1416 Views
  • 1 replies
  • 0 kudos

Problem with data transfer between 2 MCUs via I2C

Hello, dear collegues!Please help me with I2C!I use I2C to transfer data between 2 controllers: STM32F051C8T6(Master) and STM32F100C8T6 (Slave). When I use laboratory power supply, it works without some problems. But when I use external power supply ...

GKlim by Associate II
  • 1888 Views
  • 3 replies
  • 0 kudos

STM32f407G-DISC1 Technical Documents

Hi, i'm currently working with the MB997D version of the mentioned Development Kit on the caption. My main goal is working with the lis3dsh sensor on this board and then apply it to my own board, i've tried and accomplished the work with that sensor,...

EAkbu by Associate
  • 1466 Views
  • 2 replies
  • 0 kudos

STM32F746G-DISCO internal RTC not working

Hello,I am using STM32F746G-DISCO board for internal RTC. And using Keil u5 IDEI enabled the Internal RTC clock in CubeMX, set the time and date.And am using HAL_RTC_GetTime - API in while loop for reading sTime and sDate.I am monitoring sTime and sD...

Ameya M by Associate III
  • 934 Views
  • 0 replies
  • 0 kudos

I need help to configure MDMA on stm32H7

I need some help on configuring a transfer from external SDRAM buffer and LCD buffer (via FMC with Intel 8080 like interface).I've adopted the [MDMA_RepeatBlock_Rotation] as refernce example from the CUBE_H7 package.In this project for STM32H743I_EVA...

CiuppaPT by Associate III
  • 899 Views
  • 0 replies
  • 0 kudos

A PROBLEM WITH STM32F730 USING CMSIS_DSP

I had tried to compile a project with only a 64-point fft. But it turned out to be like"fft\fft.axf: Error: L6406E: No space in execution regions with .ANY selector matching arm_common_tables.o(.constdata)."I cannot believe it as I can run fft on bas...

yezoli by Associate
  • 2258 Views
  • 4 replies
  • 0 kudos

Resolved! Motor control with MCSDK

Hi everyone:We tried the MCSDK and deployed it in stm32f407. But we got a problem, for example: We use the motor control GUI trigger the motor to 20k rpm.We press the stop button.The motor go into free run status.When the motor speed decrease and not...

JamesWang by Associate II
  • 4129 Views
  • 8 replies
  • 0 kudos

Resolved! STM32L433 PWM on TIM16

Hello:There is a post on this same issue titled "TIM16 PWM signal generation...". The fix here was to set the AOE bit in the BDTR register. In that thread they were using LL.I am having a similar issue where I am unable to get the PWM output signal o...

STM32F103VCT6 more RAM+Flash than datasheet says?

Hi,today I stumbled across a problem, where I wanted to assign around 50k of RAM to FreeRTOS and I immediately got a linker error, because target ran out of RAM.I had a look at the datasheet and this says 48k RAM. I've been using a self-hacked-toget...

doss by Associate II
  • 3138 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.