STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F1: DMA read once with USART3 in LIN Bus project

Hi everyone:cherry_blossom:I start in learning LIN bus and I wrote a basic example contain master task and slave task in STM32f103 and communicate with one slave (stm32f429), the problem in stm32f1 MCU in that the DMA read just once! so the first fra...

Resolved! STM32F413 DMA1 peripheral restrictions?

I'm having trouble understanding this from the datasheet and reference.What peripherals are allowable targets for DMA1 memory-to-peripheral transfers?Thanks, Best Regards, DavePS: I tried to use a stream in DMA1 to write to a DMA control register, an...

PMOD interaface sample pin configuration code

Hi Team,Am working with STM32L4R9 Discovery board,In this SOC, PMOD interface is configured to UART in defaultWhen am trying to use this a SPI interface, am facing issueCan you pls share me the sample pin configuration for PMOD connection to configur...

AGumm by Associate II
  • 4467 Views
  • 7 replies
  • 1 kudos

Timer 2 - STM32F427ZIT6

Hello.I try timer 2 on STM32F427 and I have a problem. It ticks too quick.Here is my system clock. I have external crystal: 25MHzClock I want to: 168MHzvoid SystemClock_Config(void) { uint32_t i;   LL_FLASH_SetLatency(LL_FLASH_LATENCY_5);   if...

What happened to FSMC?

Many of the "older MCUs" like STM32F4xx had an FSMC. I've been thinking about switching to the newer STM32F7xx and have bought a Discovery board for STM32F7508, but there are no references to FSMC in the documentation. Apparently F765/7/8/9 have a "F...

DRobe.4 by Senior
  • 1616 Views
  • 2 replies
  • 0 kudos

How do I find out when DMA FIFO is empty on STM32F446?

I'm working with the STM32F446 microcontroller and I'm using UART with DMA. The size of my UART packets is contained in the 3rd and the 4th packet bytes and I would like to use FIFO on the receive stream to increase the likelihood for successfully re...

arnold_w by Senior II
  • 974 Views
  • 2 replies
  • 0 kudos

Resolved! Are the VSS and AVSS pins internally connected?

Hello community, I have a little doubt. Are all the GND pins internally connected inside the microcontroller? Is the analog reference (AVSS) internally connected with the digital one (VSS)? If it not, how is the isolation between them?I don't know wh...

Luis Ber by Associate II
  • 2530 Views
  • 2 replies
  • 0 kudos

I'm interested in using the STM32F4xx internal sensor in a deployed product. Any comments on temperature sensor accuracy and calibration are welcome and appreciated.

Per STM32F405/7 and per datasheet DocID022152 Rev 8 (stm32f4xx) ... are the values referred to in datasheet as "Temperature sensor calibration values", at addresses 0x1FFF 7A2C & 0x1FFF 7A2E (see section 5.3.22), actual factory-calibration results th...

rgodshall by Associate II
  • 1284 Views
  • 2 replies
  • 0 kudos

Resolved! Usage SRAM1, SRAM2, SRAM3 with initialized arrays

I changed linker to use all of these three memories in domain D2. Problem is next :When i put for example uint32_t tempArray[4] = {0x2B7E1516 ,0x28AED2A6 ,0xABF71588 ,0x09CF4F3C} __attribute__((section(".sram1")));this line in my code, when MCU is in...

larenge by Associate II
  • 4690 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.